This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CCS/AWR1642: How to set the contents of r4f_linker.cmd ?

Intellectual 290 points

Replies: 1

Views: 169

Part Number: AWR1642

Tool/software: Code Composer Studio

I got a error message after build my application which is based on the demo project of mmwave SDK 2.0.0.4. 

The message is shown below.

It looks like my application is growing bigger. I got the advise and modify the MEMORY MAP in the r4f_linker.cmd.

My modification is from

PROG_RAM (RX) : origin=0x00000100 length=0x0003FF00

=>

PROG_RAM (RX) : origin=0x00000100 length=0x0004FF00

Now I could successfully build the project but I am not sure I was doing the right thing.

I have the following questions and appreciate any one could help me:

1.  Is any document to guide me the 

2.  Would it cause any side-effect simply changing the length of PROG_RAM? 

3. What is the correct range of for PROG_RAM length?

  • Hi,

    Please check the memory map in the datasheet to understand the size of the memory available to you.

    Thank you
    Cesar

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.