This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

IWR1642BOOST: CAN transmit not working

Prodigy 170 points

Replies: 13

Views: 641

Part Number: IWR1642BOOST

  •  mmWave SDK 01.02.00.05

  • IWR1642BOOST

  • Silicon revision ES1.0

  • Code Composer Studio Version: 8.1.0.00011 

Hello,


I am attempting to add sending data over CAN to a program for the IWR1642BOOST.

I have added and removed resistors are instructed in the user guide.

My code to implement the CAN is largely lifted from the various example programs so DCANAppCalcBitTimeParams() is just taken from the can driver unit test program.

void Can_Initialize(void)
{
    CAN_MsgObjHandle rxMsgObjHandle;
    int32_t retVal = 0;
    int32_t errCode = 0;
    CAN_DCANMsgObjectStats msgObjStats;
    CAN_OptionTLV optionTLV;
    CAN_DCANErrorCounter errCounter;

    /* Setup the PINMUX to bring out the XWR16xx CAN pins */
    Pinmux_Set_OverrideCtrl(SOC_XWR16XX_PINC13_PADAG,
                            PINMUX_OUTEN_RETAIN_HW_CTRL,
                            PINMUX_INPEN_RETAIN_HW_CTRL);
    Pinmux_Set_FuncSel(SOC_XWR16XX_PINC13_PADAG,
                       SOC_XWR16XX_PINC13_PADAG_CAN_TX);

    Pinmux_Set_OverrideCtrl(SOC_XWR16XX_PINE13_PADAF,
                            PINMUX_OUTEN_RETAIN_HW_CTRL,
                            PINMUX_INPEN_RETAIN_HW_CTRL);
    Pinmux_Set_FuncSel(SOC_XWR16XX_PINE13_PADAF,
                       SOC_XWR16XX_PINE13_PADAF_CAN_RX);

    /* Configure the divide value for DCAN source clock */
    SOC_setPeripheralClock(gMmwMssMCB.socHandle, SOC_MODULE_DCAN,
                           SOC_CLKSOURCE_VCLK, 9U, &errCode);

    /* Initialize peripheral memory */
    SOC_initPeripheralRam(gMmwMssMCB.socHandle, SOC_MODULE_DCAN, &errCode);

    /* Initialize the DCAN parameters that need to be specified by the application */
    DCANAppInitParams(&appDcanCfgParams, &appDcanTxCfgParams, &appDcanRxCfgParams);
    gMmwMssMCB.canHandle = CAN_init(&appDcanCfgParams, &errCode);
    if (gMmwMssMCB.canHandle == NULL)
    {
        System_printf(
                "Error: CAN Module Initialization failed [Error code %d]\n",
                errCode);
        //return -1;
    }

    retVal = DCANAppCalcBitTimeParams(20000000U / 1000000,
                                      1000000U / 1000,
                                      1000000U,
                                      700U,
                                                &appDcanBitTimeParams);

    /* Configure the CAN driver */
    retVal = CAN_configBitTime(gMmwMssMCB.canHandle, &appDcanBitTimeParams, &errCode);
    if (retVal < 0)
    {
        System_printf(
                "Error: CAN Module configure bit time failed [Error code %d]\n",
                errCode);
        //return -1;
    }
    /* Setup the transmit message object */
    gMmwMssMCB.txMsgObjHandle = CAN_createMsgObject(gMmwMssMCB.canHandle, 1,
                                         &appDcanTxCfgParams, &errCode);
    if (gMmwMssMCB.txMsgObjHandle == NULL)
    {
        System_printf(
                "Error: CAN create Tx message object failed [Error code %d]\n",
                errCode);
        //return -1;
    }

    /* Setup the receive message object */
    rxMsgObjHandle = CAN_createMsgObject(gMmwMssMCB.canHandle, 2,
                                         &appDcanRxCfgParams, &errCode);
    if (rxMsgObjHandle == NULL)
    {
        System_printf(
                "Error: CAN create Rx message object failed [Error code %d]\n",
                errCode);
        //return -1;
    }
}

and it is using these parameters

static void DCANAppInitParams(CAN_DCANCfgParams* dcanCfgParams,
                              CAN_DCANMsgObjCfgParams* dcanTxCfgParams,
                              CAN_DCANMsgObjCfgParams* dcanRxCfgParams)
{
    /*Intialize DCAN Config Params*/
    dcanCfgParams->parityEnable = 0;
    dcanCfgParams->intrLine0Enable = 1;
    dcanCfgParams->intrLine1Enable = 1;
    dcanCfgParams->testModeEnable = 0;
    dcanCfgParams->eccModeEnable = 0;
    dcanCfgParams->stsChangeIntrEnable = 0;
    dcanCfgParams->autoRetransmitDisable = 1;
    dcanCfgParams->autoBusOnEnable = 0;
    dcanCfgParams->errIntrEnable = 1;
    dcanCfgParams->autoBusOnTimerVal = 0;
    dcanCfgParams->if1DmaEnable = 0;
    dcanCfgParams->if2DmaEnable = 0;
    dcanCfgParams->if3DmaEnable = 0;
    dcanCfgParams->ramAccessEnable = 0;
    dcanCfgParams->appCallBack = DCANAppErrStatusCallback;
    /*Intialize DCAN tx Config Params*/
    dcanTxCfgParams->xIdFlagMask = 0x1;
    dcanTxCfgParams->dirMask = 0x1;
    dcanTxCfgParams->msgIdentifierMask = 0x1FFFFFFF;
    dcanTxCfgParams->msgValid = 1;
    dcanTxCfgParams->xIdFlag = CAN_DCANXidType_11_BIT;
    dcanTxCfgParams->direction = CAN_Direction_TX;
    dcanTxCfgParams->msgIdentifier = 0xC1; //this is what needs to be determined
    dcanTxCfgParams->uMaskUsed = 1;
    dcanTxCfgParams->intEnable = 1;
    dcanTxCfgParams->remoteEnable = 0;
    dcanTxCfgParams->fifoEOBFlag = 1;
    dcanTxCfgParams->appCallBack = DCANAppCallback;
    /*Intialize DCAN Rx Config Params*/
    dcanRxCfgParams->xIdFlagMask = 0x1;
    dcanRxCfgParams->msgIdentifierMask = 0x1FFFFFFF;
    dcanRxCfgParams->dirMask = 0x1;
    dcanRxCfgParams->msgValid = 1;
    dcanRxCfgParams->xIdFlag = CAN_DCANXidType_11_BIT;
    dcanRxCfgParams->direction = CAN_Direction_RX;
    dcanRxCfgParams->msgIdentifier = 0xC1;
    dcanRxCfgParams->uMaskUsed = 1;
    dcanRxCfgParams->intEnable = 1;
    dcanRxCfgParams->remoteEnable = 0;
    dcanRxCfgParams->fifoEOBFlag = 1;
    dcanRxCfgParams->appCallBack = DCANAppCallback;

}

and the transmit is called in the mailbox task after transmiting data over UART, like so, where gMmwMssMCB.foldbackOverCan is of type CAN_DCANData

                    //transmit over can
                    retVal = CAN_transmitData(( CAN_MsgObjHandle*)gMmwMssMCB.txMsgObjHandle, &gMmwMssMCB.foldbackOverCan, &errCode);



                    if (retVal < 0)
                    {
                        /* Error: Unable to send the message. Setup the error code and return values */
                        System_printf(
                                "Error: failed to transmit foldback over CAN [Error code %d]\n",
                                errCode);
                    }

The program does not give any errors but if I probe the can_l and can_h ports they both just give A 2.5v level when my program is running.

What might be causing the CAN transmit to not work? Any suggestions on how to debug this?

Thanks,

Tim 

  • Hi Tim,

    Did you try running the same test with the unit test provided with the CAN driver? I would recommend you to first get the TX test working with the unit test to have a working baseline and test setup and then run your own code.

    Regards
    -Nitin
  • In reply to Nitin Sakhuja:

    Hi Nitin,

    I have now run the CAN driver unit test thanks to your help on my other post. 

    I have run the tests with a 120 ohm resistance between the can_l and can_h ports, probing both ports and also have probed the pin 1 of the CAN transceiver U3 but am not seeing any reading on the scope. 

    Running the DCAN Internal loopback test I get this on the console but only see flat voltage level on the scope.

    [Cortex_R4_0] *******************************************************
    CAN Unit Test Menu                          
    Please select the type of test to execute:  
    1. DCAN Internal loopback test              
    2. DCAN External loopback test              
    3. DCAN Parity test                         
    4. DCAN Tx/Rx test                          
    *******************************************************
    > Enter your selection: Debug: Internal loopback testing
    Debug: Number of iterations              : 100
    Debug: Number of messages transmitted    : 100
    Debug: Number of messages received       : 100
    Debug: Number of messages lost           : 0
    Debug: Number of data mismatch           : 0
    Debug: Error Status Interrupt            : 0
    
    
    Debug: Message object number             : 1
    Debug: Direction                         : Transmit
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    
    
    Debug: Message object number             : 2
    Debug: Direction                         : Receive
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    Debug: Receive & Transmit Measurements
    Debug: Rx Min:470 Max: 503 Average:476 ticks
    Debug: Tx Min:459 Max: 1340 Average:474 ticks
    
    
    Debug: Internal loopback testing for 100 iterations Passed
    Feature: Internal loopback testing: Passed
    

    Runing the DCAN External loopback test  I get this on the console and again the same reading on the scope.

    [Cortex_R4_0] *******************************************************
    CAN Unit Test Menu                          
    Please select the type of test to execute:  
    1. DCAN Internal loopback test              
    2. DCAN External loopback test              
    3. DCAN Parity test                         
    4. DCAN Tx/Rx test                          
    *******************************************************
    > Enter your selection: Debug: External loopback testing
    Debug: Number of iterations              : 100
    Debug: Number of messages transmitted    : 100
    Debug: Number of messages received       : 100
    Debug: Number of messages lost           : 0
    Debug: Number of data mismatch           : 0
    Debug: Error Status Interrupt            : 0
    
    
    Debug: Message object number             : 1
    Debug: Direction                         : Transmit
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    
    
    Debug: Message object number             : 2
    Debug: Direction                         : Receive
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    Debug: Receive & Transmit Measurements
    Debug: Rx Min:463 Max: 1344 Average:478 ticks
    Debug: Tx Min:459 Max: 476 Average:466 ticks
    
    
    Debug: External loopback testing for 100 iterations Passed
    Feature: External loopback testing: Passed

    Running the DCAN Parity test  I get this on the console and the same reading again on the scope.

    [Cortex_R4_0] *******************************************************
    CAN Unit Test Menu                          
    Please select the type of test to execute:  
    1. DCAN Internal loopback test              
    2. DCAN External loopback test              
    3. DCAN Parity test                         
    4. DCAN Tx/Rx test                          
    *******************************************************
    > Enter your selection: Debug: parity testing
    Error: ECC error status check failed. Single bit error 0 Double bit error 1 Message Number 64
    Feature: Parity testing: Failed
    Debug:CAN testing failed

    Finally running DCAN Tx/Rx test I see this in the console and still the same on the scope.

    [Cortex_R4_0] *******************************************************
    CAN Unit Test Menu                          
    Please select the type of test to execute:  
    1. DCAN Internal loopback test              
    2. DCAN External loopback test              
    3. DCAN Parity test                         
    4. DCAN Tx/Rx test                          
    *******************************************************
    > Enter your selection: Debug: External transmit testing
    Debug: External transmit testing Passed
    Debug: Number of iterations              : 1
    Debug: Number of messages transmitted    : 0
    Debug: Number of messages received       : 0
    Debug: Number of messages lost           : 0
    Debug: Error Status Interrupt            : 1
    
    
    Debug: Message object number             : 1
    Debug: Direction                         : Transmit
    Debug: Number of interrupts received     : 0
    Debug: Number of messages processed      : 1
    
    
    Debug: Message object number             : 2
    Debug: Direction                         : Receive
    Debug: Number of interrupts received     : 0
    Debug: Number of messages processed      : 0
    
    
    Debug: Receive passive error             : 0
    Debug: Transmit Error Counter            : 136
    Debug: Receive Error Counter             : 0

    Does this provide insight as to what the problem might be? 

    Thanks, 

    Tim 

  • In reply to Tim Dunham:

    Hi Tim,

    Going through the description in your previous post, it is not clear if you've followed the required ECOs as mentioned in Appendix A.4 of the following app note:

    CAN Node on AWR1642

    Could you please confirm if you've mounted 0 ohm resistor on R11 and R12 and removed R6 and R4 as required?

    Regards

    -Nitin

     

  • In reply to Nitin Sakhuja:

    Hi Nitin,

    I am using the IWR1642BOOST EVM so I followed the instructions in section 2.3.3 of that user guide http://www.ti.com/lit/ug/swru521b/swru521b.pdf and mounted 0 ohms on R11 and R12 and removed R4, R6, R28 and R63.

    Additionally, I have now tried runng the CANFD driver unit test and found that works and shows the expected output on the scope so I have tried changeing my program to use CANFD rather than CAN. This still is not working but it does give an error message. It is failing to transmit with error code -3502, which  I think is EINUSE meaning the last message is still being sent? I am only calling  CANFD_transmitData() once per frame so there should be long enough between sending the messages?

    Thanks,

    Tim

     

  • In reply to Tim Dunham:

    Hi Tim,

    You'll need an MMWAVE-DEVPACK to validate the DCAN interface since on both AWR1642BOOST and IWR1642BOOST EVMs, the DCAN lines are routed to the MMWAVE-DEVPACK. Only CAN-FD is exposed on the xWR1642BOOST which is what you got working. You'll also need to perform the ECOs mentioned in CAN Node on AWR1642 for DCAN.

    Please mark this thread resolved if your question is answered otherwise get back if more support if needed.

    Thanks

    -Nitin

  • In reply to Nitin Sakhuja:

    /* Wait for the transmit complete interrupt */
    while (gTxDoneFlag == 0);
    gTxDoneFlag = 0;

    Hi Nitin,

    I am actually still having trouble with using CAN-FD. When I run the EVM test on the CAN-FD driver unit test I do not get any results on the console and I don't see anything on the scope. When I step through the program I find that it is stuck in this while loop on line 1288:

    /* Wait for the transmit complete interrupt */
    while (gTxDoneFlag == 0);
    gTxDoneFlag = 0;

    In my program I also have the same while loop to wait for the transmit complete interrupt after the canfd transmit call and it will also get stuck in it. If I remove the loop in my program the first CANFD_transmitData() will run without returning an error but without any data being seen to be transmitted on the scope and subsequent calls will give error code -3502.

    These are the results for the other CAN-FD driver tests if they might help diagnose the problem. The external transmit test also seems to give non ideal results.

    [Cortex_R4_0] *******************************************************
    CANFD Unit Test Menu                        
    Please select the type of test to execute:  
    1. MCAN Internal loopback test              
    2. MCAN External loopback test              
    3. MCAN Parity test                         
    4. MCAN External Tx/Rx test                 
    5. MCAN EVM-EVM test                        
    6. MCAN Tx Cancel test                      
    7. MCAN Power down test                     
    *******************************************************
    > Enter your selection: Debug: Internal loopback testing
    Debug: Number of iterations              : 100
    Debug: Number of messages transmitted    : 100
    Debug: Number of messages received       : 100
    Debug: Number of messages lost           : 0
    Debug: Number of data mismatch           : 0
    Debug: Error Status Interrupt            : 0
    
    
    Debug: Message Identifier                : 670
    Debug: Direction                         : Transmit
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    
    
    Debug: Message Identifier                : 670
    Debug: Direction                         : Receive
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    Debug: Receive & Transmit Measurements
    Debug: Rx Min:1911 Max: 2803 Average:1940 ticks
    Debug: Tx Min:1090 Max: 1170 Average:1115 ticks
    
    
    Debug: Internal loopback testing for 100 iterations Passed
    Feature: Internal loopback testing: Passed

    [Cortex_R4_0] *******************************************************
    CANFD Unit Test Menu                        
    Please select the type of test to execute:  
    1. MCAN Internal loopback test              
    2. MCAN External loopback test              
    3. MCAN Parity test                         
    4. MCAN External Tx/Rx test                 
    5. MCAN EVM-EVM test                        
    6. MCAN Tx Cancel test                      
    7. MCAN Power down test                     
    *******************************************************
    > Enter your selection: Debug: External loopback testing
    Debug: Number of iterations              : 100
    Debug: Number of messages transmitted    : 100
    Debug: Number of messages received       : 100
    Debug: Number of messages lost           : 0
    Debug: Number of data mismatch           : 0
    Debug: Error Status Interrupt            : 0
    
    
    Debug: Message Identifier                : 670
    Debug: Direction                         : Transmit
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    
    
    Debug: Message Identifier                : 670
    Debug: Direction                         : Receive
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    Debug: Receive & Transmit Measurements
    Debug: Rx Min:1911 Max: 2837 Average:1931 ticks
    Debug: Tx Min:1090 Max: 1181 Average:1107 ticks
    
    
    Debug: External loopback testing for 100 iterations Passed
    Feature: External loopback testing: Passed

    No results for the parity test as it does not seem to exist in the program.

    [Cortex_R4_0] *******************************************************
    CANFD Unit Test Menu                        
    Please select the type of test to execute:  
    1. MCAN Internal loopback test              
    2. MCAN External loopback test              
    3. MCAN Parity test                         
    4. MCAN External Tx/Rx test                 
    5. MCAN EVM-EVM test                        
    6. MCAN Tx Cancel test                      
    7. MCAN Power down test                     
    *******************************************************
    > Enter your selection: Debug: External transmit testing
    Debug: Number of iterations              : 1
    Debug: Number of messages transmitted    : 0
    Debug: Number of messages received       : 0
    Debug: Number of messages lost           : 0
    Debug: Error Status Interrupt            : 1
    
    
    Debug: Message Identifier                : 193
    Debug: Direction                         : Transmit
    Debug: Number of interrupts received     : 0
    Debug: Number of messages processed      : 1
    
    
    Debug: Message Identifier                : 193
    Debug: Direction                         : Receive
    Debug: Number of interrupts received     : 0
    Debug: Number of messages processed      : 0
    
    
    Debug: Receive passive status            : 0
    Debug: Transmit Error Counter            : 8
    Debug: Receive Error Counter             : 0
    Debug: Error Logging Counter             : 0
    
    
    Debug: LEC                               : 7
    Debug: Activity                          : 1
    Debug: Error Passive                     : 0
    Debug: Warning Status                    : 0
    Debug: Bus Off Status                    : 0
    Debug: Data Phase LEC                    : 3
    Debug: Rx ESI flag                       : 0
    Debug: Rx BRS flag                       : 0
    Debug: Rx CAN FD                         : 0
    Debug: Protocol Exception Event          : 0
    Debug: TDC value                         : 14
    [Cortex_R4_0] *******************************************************
    CANFD Unit Test Menu                        
    Please select the type of test to execute:  
    1. MCAN Internal loopback test              
    2. MCAN External loopback test              
    3. MCAN Parity test                         
    4. MCAN External Tx/Rx test                 
    5. MCAN EVM-EVM test                        
    6. MCAN Tx Cancel test                      
    7. MCAN Power down test                     
    *******************************************************
    > Enter your selection: Debug: Tx Cancel testing
    Debug: Number of iterations              : 100
    Debug: Number of messages transmitted    : 100
    Debug: Number of messages received       : 0
    Debug: Number of messages lost           : 0
    Debug: Number of data mismatch           : 0
    Debug: Error Status Interrupt            : 0
    
    
    Debug: Message Identifier                : 670
    Debug: Direction                         : Transmit
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 0
    
    
    Debug: Message Identifier                : 670
    Debug: Direction                         : Receive
    Debug: Number of interrupts received     : 0
    Debug: Number of messages processed      : 0
    
    
    Debug: External loopback testing for 100 iterations Passed
    Feature: Tx Cancel testing: Passed
    [Cortex_R4_0] *******************************************************
    CANFD Unit Test Menu                        
    Please select the type of test to execute:  
    1. MCAN Internal loopback test              
    2. MCAN External loopback test              
    3. MCAN Parity test                         
    4. MCAN External Tx/Rx test                 
    5. MCAN EVM-EVM test                        
    6. MCAN Tx Cancel test                      
    7. MCAN Power down test                     
    *******************************************************
    > Enter your selection: Debug: Power Down testing
    Debug: Number of iterations              : 100
    Debug: Number of messages transmitted    : 100
    Debug: Number of messages received       : 100
    Debug: Number of messages lost           : 0
    Debug: Number of data mismatch           : 0
    Debug: Error Status Interrupt            : 0
    
    
    Debug: Message Identifier                : 670
    Debug: Direction                         : Transmit
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    
    
    Debug: Message Identifier                : 670
    Debug: Direction                         : Receive
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    
    
    Debug: CANFD Module Power Down sucessful
    Debug: CANFD Module is Wake Up sucessful
    
    
    
    
    Debug: Number of iterations              : 100
    Debug: Number of messages transmitted    : 200
    Debug: Number of messages received       : 200
    Debug: Number of messages lost           : 0
    Debug: Number of data mismatch           : 0
    Debug: Error Status Interrupt            : 0
    
    
    Debug: Message Identifier                : 670
    Debug: Direction                         : Transmit
    Debug: Number of interrupts received     : 200
    Debug: Number of messages processed      : 200
    
    
    Debug: Message Identifier                : 670
    Debug: Direction                         : Receive
    Debug: Number of interrupts received     : 200
    Debug: Number of messages processed      : 200
    
    
    Feature: Power Down testing: Passed

    Thanks,

    Tim

  • In reply to Tim Dunham:

    Hi Tim,

    We are looking into this issue and will get back to you within this week. Thanks for your patience.

    Regards
    -Nitin
  • In reply to Nitin Sakhuja:

    Hi Tim,

    Thanks for your patience. It appears that there has been some confusion over what interfaces are available on the IWR1642 and how to test them.
    1. The IWR1642 device supports CAN only so you cannot use CAN-FD on IWR1642BOOST.
    2. The automotive variant i.e. AWR1642 supports both CAN and CAN-FD.

    This confusion seems to have been created in part by the IWR1642BOOST user guide which mentions CAN-FD in Figure-1. We will update the user guide to fix this.

    Can you please confirm if you are still having issue getting the DCAN test to work?

    Thanks
    -Nitin
  • In reply to Nitin Sakhuja:

    Hi Nitin,

    So the DCAN lines will be routed through the CAN connector J3 on the IWR1642BOOST EVM and the MMWAVE-DEVPACK is not necessary?

    Yes, I am still having issues running the DCAN driver test. I get these results for each of the tests:

    1: Internal loopback

    [Cortex_R4_0] *******************************************************
    CAN Unit Test Menu                          
    Please select the type of test to execute:  
    1. DCAN Internal loopback test              
    2. DCAN External loopback test              
    3. DCAN Parity test                         
    4. DCAN Tx/Rx test                          
    *******************************************************
    > Enter your selection: Debug: Internal loopback testing
    Debug: Number of iterations              : 100
    Debug: Number of messages transmitted    : 100
    Debug: Number of messages received       : 100
    Debug: Number of messages lost           : 0
    Debug: Number of data mismatch           : 0
    Debug: Error Status Interrupt            : 0
    
    
    Debug: Message object number             : 1
    Debug: Direction                         : Transmit
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    
    
    Debug: Message object number             : 2
    Debug: Direction                         : Receive
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    Debug: Receive & Transmit Measurements
    Debug: Rx Min:470 Max: 503 Average:476 ticks
    Debug: Tx Min:455 Max: 468 Average:461 ticks
    
    
    Debug: Internal loopback testing for 100 iterations Passed
    Feature: Internal loopback testing: Passed

     2: External loopback

    [Cortex_R4_0] *******************************************************
    CAN Unit Test Menu                          
    Please select the type of test to execute:  
    1. DCAN Internal loopback test              
    2. DCAN External loopback test              
    3. DCAN Parity test                         
    4. DCAN Tx/Rx test                          
    *******************************************************
    > Enter your selection: Debug: External loopback testing
    Debug: Number of iterations              : 100
    Debug: Number of messages transmitted    : 100
    Debug: Number of messages received       : 100
    Debug: Number of messages lost           : 0
    Debug: Number of data mismatch           : 0
    Debug: Error Status Interrupt            : 0
    
    
    Debug: Message object number             : 1
    Debug: Direction                         : Transmit
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    
    
    Debug: Message object number             : 2
    Debug: Direction                         : Receive
    Debug: Number of interrupts received     : 100
    Debug: Number of messages processed      : 100
    Debug: Receive & Transmit Measurements
    Debug: Rx Min:463 Max: 1327 Average:478 ticks
    Debug: Tx Min:459 Max: 1342 Average:475 ticks
    
    
    Debug: External loopback testing for 100 iterations Passed
    Feature: External loopback testing: Passed

    3: Parity

    CAN Unit Test Menu                          
    Please select the type of test to execute:  
    1. DCAN Internal loopback test              
    2. DCAN External loopback test              
    3. DCAN Parity test                         
    4. DCAN Tx/Rx test                          
    *******************************************************
    > Enter your selection: Debug: parity testing
    Error: ECC error status check failed. Single bit error 0 Double bit error 1 Message Number 64
    Feature: Parity testing: Failed
    Debug:CAN testing failed

    4: External Transmit

    [Cortex_R4_0] *******************************************************
    CAN Unit Test Menu                          
    Please select the type of test to execute:  
    1. DCAN Internal loopback test              
    2. DCAN External loopback test              
    3. DCAN Parity test                         
    4. DCAN Tx/Rx test                          
    *******************************************************
    > Enter your selection: Debug: External transmit testing
    Debug: External transmit testing Passed
    Debug: Number of iterations              : 1
    Debug: Number of messages transmitted    : 0
    Debug: Number of messages received       : 0
    Debug: Number of messages lost           : 0
    Debug: Error Status Interrupt            : 1
    
    
    Debug: Message object number             : 1
    Debug: Direction                         : Transmit
    Debug: Number of interrupts received     : 0
    Debug: Number of messages processed      : 1
    
    
    Debug: Message object number             : 2
    Debug: Direction                         : Receive
    Debug: Number of interrupts received     : 0
    Debug: Number of messages processed      : 0
    
    
    Debug: Receive passive error             : 0
    Debug: Transmit Error Counter            : 136
    Debug: Receive Error Counter             : 0

  • In reply to Tim Dunham:

    Hi Tim,

    You still need the MMWAVE-DEVPACK to test the CAN interface on IWR1642BOOST as the CAN lines are routed to that. CAN-FD is not enabled on the IWR1642 device so you cannot use that on the IWR1642BOOST and this is something that we need to mark in the IWR1642 EVM user guide. Did you try running the CAN test with the MMWAVE-DEVPACK?

    Regards
    -Nitin

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.