This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TDC7200: when TDC7200 triggered the auto calibration

Intellectual 710 points

Replies: 1

Views: 109

Part Number: TDC7200

Which case trigger the auto calibration if no action taken with the register?

Or the chip auto calibration after boot up?

  • Piero,

    Please let me know if you would like to know which register to be used for the auto calibration.

    The results from the calibration measurements are stored in the CALIBRATION1 and CALIBRATION2 registers. Please refer to section 8.4.1 in datasheet for more details

    ---------------------------------

    Bharat Aravamudhan

    Sensor Signal Conditioning Applications

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.