This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

PGA411-Q1: PGA411-Q1: pga411 Non working

Prodigy 70 points

Replies: 5

Views: 238

Part Number: PGA411-Q1

I do it according to this circuit. The pga411 doesn't work. I don't know if there is a mistake in the circuit diagram.Rotary encoder v1.0.Sch

  • In reply to liang li:

    Thank you for sending the schematic. I will review it.

    Does the device start operating when you force FAULTRES low?
  • In reply to Clancy Soehren:

    Forced FAULTRES can not work at low ,I found that the Thermal on the back of the chip was not connected,I wonder if this is the reason.

  • In reply to liang li:

    I have a few notes about your schematic:

    - All NC pins should be connected to ground.
    - AOUT should be connected to ground.
    - C3 should be 100nF (the value wasn't shown on the schematic)

    Not connecting the thermal pad could cause an issue.
    - What is the voltage on VDD? It should be around 1.8V. If this is below 1.6V, then the device is not even powering up correctly.
    - Check the VEXT rail as well. If this is not supplied correctly, the exciter output will be unable to operate, even with FAULTRES low.
  • In reply to Clancy Soehren:

    Thank you very much for your advice.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.