This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

AWR1243: xds

Prodigy 40 points

Replies: 5

Views: 170

Part Number: AWR1243

I have a board circuit connection reference AWR1243boost

but when i connect USB ,computer can not detect the XDS110 ports?

Is there any solution?

  • Do you have CCS or XDS Emulation drivers installed on your computer?

    thank you
    Cesar
  • In reply to Cesar:

    You can download Code Composer Studio (CCS) from here: processors.wiki.ti.com/.../Download_CCS

    During the installation process, make sure to select the "mmWave Device Support" option when installing the device drivers.

    Regards,
    Kyle
  • In reply to Cesar:

    Yes, it's installed.

  • In reply to Kyle Cousino:

    CCS has been installed but the computer still can't detect the port.
    Do i need to download the firmware??
  • In reply to user5340404:

    The firmware can only be downloaded after your computer has detected the device and can be seen in Windows Device Manager.

    Are you using a custom board? There could be a problem if you did not include all of the TI devices on your board.

    Regards,
    Kyle

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.