This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

FDC1004QEVM: FDC1004QEVM, USB to I2C cut

Part Number: FDC1004QEVM

Hi,

I have a problem with the FDC1004QEVM.

When i use completly the FDC1004QEVM with a stm32, all is OK.

But, when i cut the "usb to I2c part" and i add a 5K pull up, the fdc1004 don't work.

What can i do ? 

Thanks,

Best regards,

Younesse

  • Hello,

    Our application engineer will answer your question as soon as possible.

    ---------------------------------

    Bharat Aravamudhan

    Sensor Signal Conditioning Applications

  • In reply to Bharat Aravamudhan:

    Hi Younesse,
    Are you using the sensing solutions GUI? If not, you can download the GUI from our product page.

    Best Regards,
    Bala Ravi
  • In reply to Bala Ravi:

    Hi Bala,

    Thanks for your reply.

    I didn't use the sensing solution GUI, but it works with the "usb to i2c" part.

    It doesn't work only when I cut this part.

    It's strange.

  • In reply to younesse oubane:

    Hi Younesse,
    If you're using the EVM, the device is powered up through USB. After you configure the device through I2C, it will keep the settings until its power cycled again. Can you please elaborate on what do you mean by "Cut off USB to i2C"? Also what is stm32? If you have the EVM the best way to operate is through GUI.

    Best Regards,
    Bala Ravi
  • In reply to Bala Ravi:

    Hi Younesse,
    I am going to close this thread for now. If you have any further questions please create a new thread.

    Best Regards,
    Bala Ravi
  • In reply to Bala Ravi:

    Hi Bala,

    Thanks for your reply.

    We are testing a new code.

    Best regards,

    Younesse

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.