This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TDC1000-TDC7200EVM: Delopment guidance

Prodigy 100 points

Replies: 6

Views: 312

Part Number: TDC1000-TDC7200EVM

Hi 

So I am trying to test the TDC1000-TDC7200 EVM. I have the 1 MHz sensor that comes with it. 

EXP set up. 

I have a plastic and a glass container. I am just attaching the transducer using a cellotape for now. I see the following issues:

- Tank level stays at either 2.74 cm or when I reset the TDC1000 at 2.18cm

- The TOF flight reading generally do not correlate with water level. e.g. when I have no water tank on the sensor, it still gives a reading of about 37224 ns. 

- When I put a water tank with ~4 cm water, the reading is 37233 ns

Can you suggest what I am doing wrong?

thanks and regards

  • Hi Sanjay,
    Our TDC specialist is currently out of office, and will be able to respond next week. Thanks for your patience.
    Akeem Whitehead // Texas Instruments // ASC-SENSING-SSC // Applications Engineer
    Visit our Ultrasonic Sensing FAQ page for additional information.
  • In reply to Akeem Whitehead:

    Thanks Akeem

  • In reply to Akeem Whitehead:

    Hi Akeem

    Please let me know if someone can still help me with this.

    thanks
    Sanjay
  • Hi Sanjay,

    Thanks for your patience, we have seen that the transducers do not work well if not secured properly in the containers. Please attach the transducer as in the document in the link : www.ti.com/.../snaa266a.pdf
    & try your experiment with the TDC1000-TDC7200EVM, follow the GUI instructions as the User's guide you should be able to measure the tank level.

    ---------------------------------

    Bharat Aravamudhan

    Sensor Signal Conditioning Applications

  • In reply to Bharat Aravamudhan:

    Thanks Bharat

    regards

  • In reply to Sanjay Gupta96:

    You are welcome

    ---------------------------------

    Bharat Aravamudhan

    Sensor Signal Conditioning Applications

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.