This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

Choosing the right DSP + Evaluationboard for Sensorapplication

Prodigy 20 points

Replies: 3

Views: 414

Hello Community,

I´m looking for a DSP + Evaluationboard. I need 4 analog in- and outputs. At least for two in- and outputs i need 24 bit resolution converters.
 
I want to generate a sin- and cosinwave with this DSP. The DSP shoud be able to shift the Phase of the Signals.
This DSP should be able to realize a VCO with 4 different sin- and  4 cosinus outputs and 4 Voltage controll Inputs to realize a Phase Locked Loop.
I want to realize a Quadrature demodulation, the DSP should be able to do multiplications.
 
The DSP (general purpose) should be free programmable.
 
Are there Evaluationboards with 24 bit resolution converters or Evaluationboards which can be extended with those 24-bit converters?
 
I´m looking forward to hearing from you.
 
Best Regards
Viktor Heinz
  • Hi Viktor,

    On the embedded/real-time control side of processors you have C2000 devices (www.ti.com/.../overview.html) and the processor family you'd probably want is F2837xD (www.ti.com/.../tms320f28379d.pdf). For EVMs for this device you have either the Lauchpad (www.ti.com/.../LAUNCHXL-F28379D) or the ControlCard (www.ti.com/.../tmdscncd28379D). The launchpad would be able to directly mate with an external EVM if it is in 'boosterpack' format.

    You would need an external ADC to do sensing at 24-bit resolution, but auxiliary inputs can be done via on-chip ADC (12-bit or 16-bit). 24-bit outputs would need to be via external EVM, but auxiliary outputs can be achieved via a 12-bit DAC or PWM module.

    If you needed more processing power, you might look at the Beagle Bone (https://beagleboard.org/bone). This would be able to directly mate with an external EVM if it was in 'cape' format.

    Did a reply answer your question? If yes, please click the "Resolved" button located at the bottom of that post.
    Visit these helpful C2000 Links!

    C2000 TI Wiki Pages
    TI Forum Sitemap

    ControlSUITE
    C2000 Getting Started

    CLA FAQs
    Workshop Material!

  • Hey Devin,
     
     
    Thank you for your respnose.
    Is it possible to extend one of the Evaluation Kits /Board below with those 24-bit ADC (maybe with Codecs)
     
    Best Regards
    Viktor Heinz
     
    Gesendet: Mittwoch, 05. Dezember 2018 um 21:26 Uhr
    Von: "Devin Cottier" <bounce-1120590@mail.e2e.ti.com>
    An: mmwave_sensors_forum@mail.e2e.ti.com
    Betreff: Sensors forum: Choosing the right DSP Evaluationboard for Sensorapplication

     

    A Message from the TI E2E™ Community
    Texas Instruments

     

    Devin Cottier replied to Choosing the right DSP Evaluationboard for Sensorapplication.

    Hi Viktor,

    On the embedded/real-time control side of processors you have C2000 devices (www.ti.com/.../overview.html) and the processor family you'd probably want is F2837xD (www.ti.com/.../tms320f28379d.pdf). For EVMs for this device you have either the Lauchpad (www.ti.com/.../LAUNCHXL-F28379D) or the ControlCard (www.ti.com/.../tmdscncd28379D). The launchpad would be able to directly mate with an external EVM if it is in 'boosterpack' format.

    You would need an external ADC to do sensing at 24-bit resolution, but auxiliary inputs can be done via on-chip ADC (12-bit or 16-bit). 24-bit outputs would need to be via external EVM, but auxiliary outputs can be achieved via a 12-bit DAC or PWM module.

    If you needed more processing power, you might look at the Beagle Bone (https://beagleboard.org/bone). This would be able to directly mate with an external EVM if it was in 'cape' format.

     

     

     

    Did a reply answer your question? If yes, please click the "Resolved" button located at the bottom of that post.
    Visit these helpful C2000 Links!

    C2000 TI Wiki Pages
    TI Forum Sitemap

    ControlSUITE
    C2000 Getting Started

    CLA FAQs
    Workshop Material!

     

     

    You received this notification because you subscribed to the forum.  To unsubscribe from only this thread, go here.

    Flag this post as spam/abuse.

    refid:24c72bed-b8bf-4554-8d3d-ed7e6d37e7c0

  • In reply to Viktor Heinz:

    Hi Viktor,

    Take a look at the BOOSTXL-ADS1219. We do not have any CODEC boards that fit the 'booster pac' form factor.

     

    Regards,

    Tom

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.