This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

IWR1642BOOST: Error using bin file

Expert 1240 points

Replies: 3

Views: 74

Part Number: IWR1642BOOST

Hi,

when I try to load the .bin file through the CCS I am getting this error once the mss.bin file is loaded into mmwave IC.

maave sdk 2.0.0.4, recent IWR toolbx i am using and CCS 8.1. IWR1642 VER B

[Cortex_R4_0] xdc.runtime.Main: "platform/mmwave_xwr16xx.c", line 1342: assertion failure
Exception occurred in ThreadType_Main.
Main handle: 0x0.
Main stack base: 0x800d1a0.
Main stack size: 0x1000.
R0 = 0x00000000 R8 = 0x00000000
R1 = 0x0800bcf8 R9 = 0xfffffffe
R2 = 0x080001fd R10 = 0x08005424
R3 = 0x0000000a R11 = 0x0000053e
R4 = 0x00000000 R12 = 0x0000f683
R5 = 0x0800bfdc SP(R13) = 0x08005370
R6 = 0x0000004c LR(R14) = 0x000128af
R7 = 0x00000000 PC(R15) = 0x000112bc
PSR = 0x400c019f
DFSR = 0x00000000 IFSR = 0x00000000
DFAR = 0x00000000 IFAR = 0x00000000
ti.sysbios.family.arm.exc.Exception: line 209: E_undefinedInstruction: pc = 0x000112bc, lr = 0x000128af.
xdc.runtime.Error.raise: terminating execution

every time, though I power off the mmwave still this occurs. Some times this works properly.

Kindly help me to get rid of this issue.

  • Hello Karthik,

    The bin file is flashed using Uniflash. It is not loaded with CCS. Please follow the instructions in the lab setup guide.

    Regards,
    John
  • In reply to JohnH:

    Hi, I am loading and folllowing setugp gide. I am trying to load .xe4f for debug session using CCS since I am displaying some measued valued on console i Wwill see it on console if I run through CCS.
  • In reply to karthik s60:

    Hi Karthik,

    When posting queries, please use a descriptive title (i.e. not just "IWR1642") and include the following:

    - Version of mmWave SDK & TI RTOS you are using.
    - Details of board platform (EVM & its revision) you are using.
    - Silicon revision of your device.
    - Version of compiler and Code Composer Studio
    - For API specific issues, please provide the application source code used.
    - For run-time issues, please provide a detailed description of the problem and the expected behavior.
    - Provide/attach relevant Message Log and debug information or screen captures of the issue.

    More information provided with first post will help us better understand the nature of query and speed up the response time.

    Regards,
    John

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.