This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

AWR1243: AWR1243

Intellectual 430 points

Replies: 11

Views: 561

Part Number: AWR1243

Hello

I am designed a cascaded radar with 2 AWR1243 (one is Master and other is Slave). Each AWR1243 is powered by 4 LDO and the PMIC not used.

The pins that are connected to 60-pin connector are:LVDSs (Data[0-3], CLK, Frame CLK, Valid), SPIs( CS, MISO, MOSI, CLK), Host INTR(p6), NRST_MCU and NERR_OUT(N8) and there is no other connection to outside in the cascaded AWR1243.

I want to design an Capture card like DCA1000EVM Kit.
Are the connected pins sufficient for proper radar functionality?

For digital frame synchronization, I got an output from SYNC_OUT(P11) and gave it to SYNC_IN pins( N10) on both of Master and Slave with equal length.In DCA1000EVM Kit, SYNC_IN pin of AWR1243boost is connected through DMM_MUX_CTL.Duo to synchronization done, Is it necessary to connect SYNC_IN to Capture card? or is it necessary to connect SYNC_OUT to Capture card?

Pins of MCU_CLKOUT(N9) and WARM_RESET(N12) of AWR1243boost are not connected to DCA1000EVM. Does not create disrupting in programming and functionality of cascaded AWR1243 without connecting of these pins?

Thanks

   

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.