• Resolved

LDC1614EVM: Graph and Inductance

Expert 1200 points

Replies: 4

Views: 72

Part Number: LDC1614EVM

Dear Bala and Clancy

HERE ARE MY QUESTIONS: 

1. I am using a 8 layer coil which has an inductance of 1000uH. In data streaming shown the vertical scaling maximum reach to almost 1200uH. Is this acceptable? 

2. In the configuration, Sensor Filter Bank (Series Inductance) is it remain 0 or should i put the inductance value of the coil?