This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

IWR1642BOOST: IWR1642 and STM32

Prodigy 10 points

Replies: 1

Views: 64

Part Number: IWR1642BOOST

How to connect the IWR1642 to the STM32 controller using Uart, while having the ability to configure the IWR board and get data about the objects from IWR board? Does this board have the ability to use separate connectors to configure and retrieve data, for example, use SPI for configuring and RS232 for receiving data?

  • Hi Andrey,

    We have a reference design for IWR1443BOOST and an MSP432 Launchpad which I'd recommend looking at. The TIDEP-0091 sends range information from the sensor to the MSP432 over SPI and then outputs the data from the MSP432 via UART.


    Cheers,
    Akash

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.