This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CCS/AWR1642BOOST: Running SRR Demo (TIDEP - 0092) without opening the GUI

Prodigy 180 points

Replies: 1

Views: 57

Part Number: AWR1642BOOST

Tool/software: Code Composer Studio

Hi all,

I have the same question as the thread : http://e2e.ti.com/support/sensors/f/1023/p/727721/2689279 I would like to run the SRR demo without Matlab GUI

the last answer in the above thread says there is a "UART_read()" in "CLI_task()" in file "mmwave-sdk-install\ti\utils\cli\src\cli.c" 

but I can't find where the SRR demo code uses the CLI_task() or UART_read() function.

I wonder where should I bypass the CLI (CLI_task) and then call the AdvanceframeCfg and sensorstart functions

hope you can help me figure this out, thanks a lot!!

BR

Brian

  • Hi,
    If you wish to add CLI bypass feature to the application then refer this application where it has the hardocded CLI commands in the application itself and on boot up it invokes those CLI.
    dev.ti.com/.../node

    [cli.c: radarCmdString]

    Regards,
    Jitendra

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.