This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CCS/IWR6843ISK: IWR6843 3D debug mode

Intellectual 725 points

Replies: 31

Views: 834

Part Number: IWR6843ISK

Tool/software: Code Composer Studio

Hi,

I have the IWR6843 board, and i want to use it with mmwave industrial toolbox 3_3_1 lab 20.

At the past i used to use debug mode at previous board of the mmwave.

I experience difficulties when trying to use lab20 at the mentioned toolbox at debug mode.

The lab20 has two sub projects.,both passed compilation.

In order to deal at debug mode,i did the following:

1.load jumper on SOP2

2.connect uniflash

3.power cycle of the board

4.start burning the C:\ti\mmwave_sdk_03_01_01_02\packages\ti\utils\ccsdebug\xwr68xx_ccsdebug.bin

5.it passed successfully->removing the jumper from the SOP2

6.CCS->compiling the projects DSS MSS->successfully

7.creating target configuration file->load the resulting file->gather files to group->connect to target

8,when connecting to target ,the CCS gets stuck.

I've attached the relevant screenshots.

Please assist.

  • Hi Gil,

    Can you confirm you have power cycled your board after flashing your board and removing the SOP2 jumper?


    Cheers,
    Akash
  • In reply to Akash Gondalia:

    Hi Akash,
    I confirm i did it.
    tries this scenario three times.
    Gil
  • In reply to gil albo:

    Hi Gil,

    It appears your Target Config File (.ccxml) is for AWR1443, make sure you select IWR6843 for this.


    Cheers,
    Akash
  • In reply to Akash Gondalia:

    Hi Akash.
    I've verified that the target configuration file is for IWR6843.
    The image shows the mouse somehow in focus on the AWR1443, but only the IWR6843 is checked.
    please assist.
  • In reply to gil albo:

    Hi Gil,

    When you say it is getting stuck, do you mean it is not loading an executable or that it requires an update or something else? Would you be able to post a screenshot of the actual error?


    Cheers,
    Akash
  • In reply to Akash Gondalia:

    Hi Akash,

    All the pictures that i've attached above show the situation.

    anyway,

    here are the messages again:

    I'm using the IWR6843ISK with lab20 which from the mmwave toolbox 3_3_1

    i have the latest mmwave SDK mmwave_sdk_03_01_01_02

    the projects MSS and DSS passed compilation.

    I've flashed the ccsdebug of the IWR6843 successfully and removed the SOP2 jumper afterwards.

    created new target configuration file when selecting only the IWR6843  and XDS110 USB debug mode.

    I've saved this ccxml file.

    then clicked on the test connection button ,and the result is:

    [Start: Texas Instruments XDS110 USB Debug Probe]

    Execute the command:

    %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

    [Result]

    -----[Print the board config pathname(s)]------------------------------------

    C:\Users\GIL~1.ALB\AppData\Local\TEXASI~1\

       CCS\ti\1\0\BrdDat\testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 100- or 510-class product.

    This utility will load the adapter 'jioxds110.dll'.

    The library build date was 'Jan 24 2019'.

    The library build time was '14:27:46'.

    The library package version is '8.0.903.6'.

    The library component version is '35.35.0.0'.

    //////////////////////////////////////////////////////////

    Then ,I launched that target file ccxml and grouped the two

    then , a message appear:

    when clicking updated, the device is stuck forever.

    Please assist.

    Gil

  • In reply to gil albo:

    Hi Gil,

    Does your "Test Connection" Report have any more information? You may just have a bad USB cable.

    Have you been able to run other demos and labs previously?


    Cheers,
    Akash
  • In reply to Akash Gondalia:

    Hi Gil,

    Since we haven't heard from you I'm going to close this thread but if you still have questions then feel free to open up a new one!


    Cheers,
    Akash
  • In reply to Akash Gondalia:

    Hi Akash.
    How are you ?
    The problem wasn't solved.
    I was provided with new IWR6843 board.
    I successfully flashed the device with two bin files(one per trial).
    one provided with lab20, and another that i generated from my lab20 project.
    in both cases, the GUI was functioning well.

    But when trying to debug, the issues mentioned above remained.
    i did update to the ccs.
    i used another usb cable.
    i used new project ,importing lab 20.

    directions ?
  • In reply to gil albo:

    Hi Gil,

    Can you try this on a different PC?

    This is different from what you had first said, you will need to flash the CCS Debug Firmware in order to debug this on CCS.

    Have you tried running the board with any of the prebuilt binaries included in either the mmWave-SDK (recommended starting point) or the Industrial Toolbox?


    Cheers,
    Akash

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.