This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CCS/IWR6843ISK: IWR6843 3D debug mode

Intellectual 725 points

Replies: 31

Views: 961

Part Number: IWR6843ISK

Tool/software: Code Composer Studio

Hi,

I have the IWR6843 board, and i want to use it with mmwave industrial toolbox 3_3_1 lab 20.

At the past i used to use debug mode at previous board of the mmwave.

I experience difficulties when trying to use lab20 at the mentioned toolbox at debug mode.

The lab20 has two sub projects.,both passed compilation.

In order to deal at debug mode,i did the following:

1.load jumper on SOP2

2.connect uniflash

3.power cycle of the board

4.start burning the C:\ti\mmwave_sdk_03_01_01_02\packages\ti\utils\ccsdebug\xwr68xx_ccsdebug.bin

5.it passed successfully->removing the jumper from the SOP2

6.CCS->compiling the projects DSS MSS->successfully

7.creating target configuration file->load the resulting file->gather files to group->connect to target

8,when connecting to target ,the CCS gets stuck.

I've attached the relevant screenshots.

Please assist.

  • In reply to Akash Gondalia:

    Hi Akash,
    i dont have the resources to check on another pc.
    few months ago, i've worked with the 2Tx isk board for people counting and other labs, and it was good at debug mode.
    Can you check on the IWR6843ODS-ISK board with the lab20, if it's possible to work on debug mode ?
    BR
    Gil
  • In reply to gil albo:

    Hi Gil,

    From your last screenshot, you need to update the debug probe. Have you done that? (Click update in the prompt).

    Regards,
    Justin
  • In reply to Justin Curewitz:

    Hi Justin.
    I did the update stage and while doing this, the CCS got stuck.
    I did it several times, and also on the previous IWR6843ISK board .
    Also, i checked for updates for the CCS.
    The cable is new and arrived at the package of the module.

    Can you verify whether the debug mode is functioning at the IWR6843 ?
    Thank you
    Gil
  • In reply to gil albo:

    Hi Gil,

    I can confirm that debug mode works with CCS - I have used it myself yesterday. However, I am using CCS 8.3 - Please check your version by clicking "Help->About Code Composer Studio" in the top left.

    Please check some of the hardware settings on the board:
    Following the People Counting user's guide, ensure the device is in functional mode. Check both the SOP pins and the Switches.

    Regards,
    Justin
  • In reply to Justin Curewitz:

    Hi Justin,
    i have the Version: 8.3.0.201810301800
    I've followed the instructions as described in the manual, and still it gets stuck .
    I'll try again.

    Gil
  • Guru 298315 points

    In reply to gil albo:

    Gil,
    Please run the JTAG connectivity test and post the results:
    dev.ti.com/.../node

    Thanks
    ki

    -----------------------------------

    Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.

    Having CCS problems? Check out the CCS Troubleshooting Guide

    Looking for CCS Training/Documentation? Check out the CCS Resources page

    Curious about the status of a bug and know the tracking ID? Track it via the public bug tracking portal

    NOTE: When a bug is filed and a tracking ID is provided, the thread may then be suggested as "TI Thinks Resolved". Why? Please read the first FAQ of the CCS Forum Guidelines & FAQ

  • In reply to Ki:

    Hi Ki-Soo,

    I did the Jtag test many times,

    0.I'm using the IWR6843ODS-ISK board with XDS110 usb debug mode.

    The SDK used is 3_1_1_2

    The CCS is Code Composer Studio, Version: 8.3.0.201810301800 ,Build id: N201810301800

    1.I've loaded the C:\ti\mmwave_sdk_03_01_01_02\packages\ti\utils\ccsdebug\xwr68xx_ccsdebug.bin

    first connected SOP2->openend uniflash->pressed on the reset button->flashed the bin file xwr68xx_ccsdebug.bin->program load completed successfully->turn off the board power->removed the SOP2 jumper.

    2.The projects (DSS & MSS of lab20 were built succussfuly)

    3.I've created new target configuration file

    *Connection:XDS110 usb debug mode.

    *Board of device: IWR6843 (just this.I've verified no other board was checked)

    *saved the configuration file

    *pressed the test connection->Here's the output:

    [Start: Texas Instruments XDS110 USB Debug Probe_0]

    Execute the command:

    %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

    [Result]


    -----[Print the board config pathname(s)]------------------------------------

    C:\Users\GIL~1.ALB\AppData\Local\TEXASI~1\
    CCS\ti\1\0\BrdDat\testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 100- or 510-class product.
    This utility will load the adapter 'jioxds110.dll'.
    The library build date was 'Jan 24 2019'.
    The library build time was '14:27:46'.
    The library package version is '8.0.903.6'.
    The library component version is '35.35.0.0'.

    Here's the ouput 

    [Start: Texas Instruments XDS110 USB Debug Probe_0]

    Execute the command:

    %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

    [Result]


    -----[Print the board config pathname(s)]------------------------------------

    C:\Users\GIL~1.ALB\AppData\Local\TEXASI~1\
    CCS\ti\1\0\BrdDat\testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 100- or 510-class product.
    This utility will load the adapter 'jioxds110.dll'.
    The library build date was 'Jan 24 2019'.
    The library build time was '14:27:46'.
    The library package version is '8.0.903.6'.
    The library component version is '35.35.0.0'.

    4.The CCS is stuck...

    5.When Flashing my device not in debug mode,the board is functioning well->Therefore the cable is ok (it also arrived from TI with the device)

    Please direct me.

    Gil

  • Guru 298315 points

    In reply to gil albo:

    gil albo

    Here's the ouput 

    [Start: Texas Instruments XDS110 USB Debug Probe_0]

    Execute the command:

    %ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -S integrity

    [Result]


    -----[Print the board config pathname(s)]------------------------------------

    C:\Users\GIL~1.ALB\AppData\Local\TEXASI~1\
    CCS\ti\1\0\BrdDat\testBoard.dat

    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 100- or 510-class product.
    This utility will load the adapter 'jioxds110.dll'.
    The library build date was 'Jan 24 2019'.
    The library build time was '14:27:46'.
    The library package version is '8.0.903.6'.
    The library component version is '35.35.0.0'.

    4.The CCS is stuck...

    There is no error message? It never returns? Are you forced to terminate the test manually?

    Also, please try updating your TI emulators component to the latest version (Chec for CCS Updates)

    -----------------------------------

    Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.

    Having CCS problems? Check out the CCS Troubleshooting Guide

    Looking for CCS Training/Documentation? Check out the CCS Resources page

    Curious about the status of a bug and know the tracking ID? Track it via the public bug tracking portal

    NOTE: When a bug is filed and a tracking ID is provided, the thread may then be suggested as "TI Thinks Resolved". Why? Please read the first FAQ of the CCS Forum Guidelines & FAQ

  • Hi again,
    This is the message.
    When debugging with other type of EVM of TI (2Tx antenna board mmwave) ,the message at the test connection ended with success.
    This doesn't happen here.

    When checking for updates i get the messages:
    Some sites could not be found.  See the error log for more detail.
    No repository found at file:/C:/Users/Gil.Albo/AppData/Local/Temp/traceplugin-Repo/.
    No repository found at file:/C:/Users/Gil.Albo/Downloads/CCS8.2.0.00007_win32%20(1)/CCS8.2.0.00007_win32/baserepo/p2appfRepo/.

    What do you recommend ?

  • Guru 298315 points

    In reply to gil albo:

    Ah, I see you are using 8.2.0. Could you try updating to 8.3.1? Or better yet, 9.0.1. I believe for the latter, you need to do a clean install of 9.0.1.

    -----------------------------------

    Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.

    Having CCS problems? Check out the CCS Troubleshooting Guide

    Looking for CCS Training/Documentation? Check out the CCS Resources page

    Curious about the status of a bug and know the tracking ID? Track it via the public bug tracking portal

    NOTE: When a bug is filed and a tracking ID is provided, the thread may then be suggested as "TI Thinks Resolved". Why? Please read the first FAQ of the CCS Forum Guidelines & FAQ

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.