This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

IWR1642BOOST: Sensor sending NAN (not a number) values in target data after a week or long run

Intellectual 595 points

Replies: 5

Views: 88

Part Number: IWR1642BOOST

Hi all,

I'm using IWR 1642 BOOST for people count application. I'm checking the tlv data for target x,y positions.

Sensor seems to function well in the beginning. After a few days or a week, it is sending -nan values for posx,posy values. 

Therefore the people count seems low and there is no target seen on matlab screen except point  cloud data. When the sensor has been rebooted, it functions normally again (for a week may be ).

I'm receiving the tlv data and printing it in my program. Here is the sample output. 

Can anyone tell me why is this occurring and what is the solution to this problem?

Thanks,

radha.

  • Hi Radha,

    We will look into this - it may take about a week.

    Regards,

    Justin

  • In reply to Justin Curewitz:

    Hi Radha,

    The IWR1642 version of the demo uses an old version of GTrack. To get the latest version, which should remove this issue, please ensure you have the latest mmWave SDK (3.2.0.4), and recompile the demo using the GTrack library from this SDK.  GTrack is a library, so you just need to change the linker file path for GTrack.  This can be done through project properties in code composer studio.

    Regards,

    Justin

  • In reply to Justin Curewitz:

    Hi Justin,

    Thanks for your quick response. I will try the fix you stated above and test for about a week or more and then update you.

    Thanks,

    radha.

  • In reply to Justin Curewitz:

    Hi Justin,

    Is it okay to just link the Gtrack library from latest sdk (or ITB) into the demo code from previous version of sdk (or ITB) as you suggested?

    Or is it better to build the demo code from the latest sdk or ITB which has this GTrack fix?

    Now i have just tried the first method as you suggested but will this lead to any performance issues?

    Thanks,

    radha.

  • In reply to radha:

    Hi Radha,

    You can use the prebuilt GTrack lib binary in the SDK. This is found at:

    <MMWave_SDK_Directory>\packages\ti\alg\gtrack_default\lib\libgtrack2D.aer4f

    Regards,

    Justin

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.