• Resolved

AWR1642BOOST:The detection range of AWR1642,AWR1443,AWR1243 .How does the maximum IF affect the performance of these modules

Prodigy 30 points

Replies: 3

Views: 109

Part Number: AWR1642BOOST

Hi, I have encountered several problems when learning millimeter-wave radar. I hope to get some help.

Q1:The detection range of AWR1642,AWR1443,AWR1243,How to calculate it?

Q2:How does the maximum IF affect the performance of these modules?

Thank you!

  • Please see the mmwave training series

    https://training.ti.com/intro-mmwave-sensing-fmcw-radars-module-1-range-estimation?cu=1128486

    It explains the equations to determine the theoretical max range.

    In practice, the max range depends on several factors: RCS of object detected, memory, Tx/Rx power ...

    The AWR1443 can usually be used to detect cars up to 50-60 meters.

    The AWR1642 can be used to detect cars up to 80-100 meters

    The AWR1243 can be used to detect cars up to 150 meters

    Thank you

    cesar

  • In reply to Cesar:

    Hi ,Thank you for your answer.

    Do you know which parameters of the MMW module are affected by the maximum if? Such as the measurementof range,velocity, direction.

    Is the maximum IF the same as the IF bandwidth?

  • In reply to user6130952:

    Yes,

    For max IF you can use the value of IF provided in the datasheet.

    The parameters affected by max IF are provided in the mmwave equations described in the training I mentioned

    Thank you

    Cesar