• TI Thinks Resolved

Compiler/AWR1642: CAN

Expert 1135 points

Replies: 5

Views: 119

Part Number: AWR1642

Tool/software: TI C/C++ Compiler

Hi,

I am using awr1642 boards. i am using two boards for CAN communication using canfd driver provided in SDK  with type calssic can.

from one board 128 bytes of data is sending.

from second board i am trying to receive the same data by calling CANFD_getData() function. I am able to receive 64 bytes of data only.

I am not understanding the flow here. rxDataLength is always 8 bytes. but it is storing 64 bytes of data. I printed rxData upto 128 bytes.

after 64 bytes printing it is not getting next 64 bytes. 

Please guide me with any receive program to receive complete data. 

Thanks and regards,

K Subrahmaniam

  • Hi,

    WIll get back to you next week

    thank you

    Cesar

  • In reply to Cesar:

    Hello Subrahmaniam,

    To send out 128bytes of data over the CANFD interface, you will need to send out the data in chunks of 64 bytes . What this means is you will need to call CANFD_TransmitData() in a loop till all data is sent out .

    This was already indicated to you in your previous post :

    https://e2e.ti.com/support/sensors/f/1023/t/830811?tisearch=e2e-sitesearch&keymatch=%252520user%25253A354388

    Please refer to the example "Object Data Over CAN" in TI Resource Explorer . Refer to function Can_Transmit_Schedule() in mss_main.c which has the reference for sending the data over CANFD in chunks.

     

    Thanks,

    Raghu

  • In reply to Raghunandan Kamath:

    Hi,

    Thank you .

    I am able to send 128 bytes of data over classical CAN. In PCAN tool i am receiving the same 128 bytes of data.

    Now i connected two AWR 1642 boards. one board sending same 128 bytes data over classical can.

    from second board i am trying to receive the data of 128 bytes. I am able to receive only 64 bytes of data. 

    i tried all the ways. please guide me any code to receive complete data. 

    Thanks and regards,

    K Subrahmaniam

  • In reply to ks prasad:

    Hi,

    It's Ok now i am able to receive 128 bytes data. but another problem is one set of 8 bytes is receiving and one is missing because

    of synchronization between sender and receiver. I tried with different task sleeps. please guide me to get the synchronization.

    thanks and regards,

    K Subrahmaniam

  • In reply to ks prasad:

    Hi Subramaniam,

    You can add code to wait for pending transmission before transmitting new message on the CAN interface. This should help with the synchronization. 

    Thanks,

    Raghu