• TI Thinks Resolved

AWR1843: BIST test

Prodigy 200 points

Replies: 7

Views: 144

Part Number: AWR1843

Hi Experts,

I'm trying to understand how to use the BIST function in the AWR1843,
but the documentation is not clear for me and no APIs are provided.
Would you please provide sample code to run BIST?

Best Regards,
Chunzhou

  • Hi Chunzhou San,

    BSS does the internal test (BIST: built-in self-test) by itself at boot time. Status of this can be known by rlGetRfBootupStatus API.

    Sample code is available in mmwavelink test application (link_test.c).

    Regards,

    Jitendra

  • In reply to Jitendra Gupta:

    Hi, Jitendra-san

    I understand that BSS automatically does BIST at boot time.

    Do MSS and DSS do BIST by itself as well as BSS?

    What is the API to get the result?

    Regards,

    Chunzhou

  • In reply to chunzhou:

    Hi Chunzhou-san,

    MSS and DSS is user space; in case of AWR1843 the user can write required test by their own to do those tests.

    AWR1843 bootloader does the boottime tests and if any of those fails then instead of switching to application it raises nError line high as notification of test failure. So if application bootup correctly that means boottime test by MSS bootloader passed. List of these tests are mentioned in the safety manual and in ICD document (SBID 0x5000).

    Regards,

    Jitendra

  • In reply to Jitendra Gupta:


    Hi, Jitendra-san

    - Does [AWR1843 bootloader does the boottime tests] include both MSS and DSS tests? Or is it only MSS test?
      The register of [SBID 0x5000] seems to include only MSS modules.

    - Does the user need to create DSS boottime test program?


    Regards,

    Chunzhou

  • In reply to chunzhou:

    Hi Chunzhou-san,

    Bootloader does only MSS test.

    user needs to create a DSS boottime test program.

    Regards,

    Jitendra

  • In reply to Jitendra Gupta:

    Hi Jitendra-san,

    Would you please provide sample code to run BIST of DSS and list of thease tests.

    Regards,

    Chunzhou

  • In reply to chunzhou:

    Hi Chunzhou-san,

    One of TI representative is following this query with us offline.

    I'm parking this thread here, you can re-open if required.

    Regards,

    Jitendra