Other Parts Discussed in Thread: TIDA-00824, TIDA-00721, CC2640R2F, TMP117
I am using LMT70 temperature sensor for measuring human body temperature.
What are the human body locations available to fix this sensor?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using LMT70 temperature sensor for measuring human body temperature.
What are the human body locations available to fix this sensor?
Hi Naga,
Yes, it is possible to design the sensor onto a patch to stick onto the body as long as it makes good contact to the skin. Please refer to TIDA-00721 which is a TI Design for a temperature sensing patch. Additionally, the application note SNIA021A describes layout considerations for wearable temperature sensors for the human body.
Regards,
Audrey
Fine sir.
The TIDA-00721 temperature sensing patch using NFC application.
Is it possible to transmit the temperature data via bluetooth to a smartphone?
Can i use bluetooth Microcontroller chip to interface with LMT70 for this application?
Regards,
Nagarajan
Naga,
LMT70 is an analog sensor. Once you have converted the analog output to digital you can choose whatever means to transmit wirelessly.
-Kelvin
Hi Sir,
I have interfaced LMT70 temperature sensor with CC2640R2F bluetooth MCU which has 12 bit ADC.
Will LMT70 sensor support 12 bit ADC type?
- Naga
Hi Sir,
Is it possible to increase the range of NFC communication between temperature sensing patch and smartphone?
- Naga