I am trying to collect the Raw ADC Data using MATLAB instead of the Radar Studio. Is there an easy to understand method to do it?
I have gone through the "Controlling mmWave Studio from Matlab" section in the user guide of mmWave Studio GUI. But I am not sure how it is working. I have created the two scripts and saved them in the location of RtttNetClientAPI.dll. Next, typed RSTD.NetStart() in the LUA window of Radar Studio and finally, ran the script Init_RSTD_Connection. I don't get any error nor any response. The Matlab is just busy since then. DO I need to go something? As in after doing this process, do I have to do the configuration setup in Matlab and then so the Frame Trigger as done in the normal case?
Many Thanks