Tool/software: Linux
What is a clutter and how to remove it? I tried to play with the configuration parameters, it seems I cannot find a way to remove the "noise": there is always something "seen" something about 1 meter in front of the radar, while there is nothing before the radar sensor, this is especially "obvious" if the sensor is under sunlight. If the sensor is put under shade or indoors, the situation is better. The horizontal view area is 180 degree and the vertical area is 60 degree. The "cfarCfg" is set to "0 2 8 4 3 0 768".