Other Parts Discussed in Thread: , UNIFLASH
We have had many problems with connecting the AWR1243 and DCA1000 with our computers in mmWave Studio
- the SPI connect button (or command in Lua scripts called “ar1.PowerOn”) does not work. We keep getting error: Run out of time
- This recently has been happening more than half the time we try to connect.
- the Ethernet connection
- Keep getting errors that Ethernet connection is down. “Ethernet plug is disconnected”
- The Ethernet chord is definitely plugged in and based on information we see in wireShark as well as LED's on the ethernet port, the computer is seeing the Ethernet connection
In both these cases, turning on and off everything tends to help the situation, but not always. If there is anything that is known to fix these connection issues, it would be greatly appreciated!
YS
AWR1243 version:
AWR1243BOOST serial numbers: 5099100248, and 5099100293
DCA1000 version:
DCA1000 serial numbers: 1918DCA1000EVM0230, and 1918DCA1000EVM0100
Mmwave Studio version: 1.0.0.0
Laptops:
(1) Windows 10 home, intel i5-7200U CPU @2.5GHz 2.7GHz, 8 GB memory
(2) Windows 8.1, intel i5-425U CPU @ 2.4GHZ 2.4GHz, 8GB memory