fig1 Configuration
fig2 Result when Config 1/2
fig3 Result when Config 2/2
I am trying to cnfig 1 BMP frame,see fig1.
my frame is Chirp0_Chirp1_Chirp0_Chirp1_.....(128 cycles), and phase settings by BMP config are:
Chirp0:TX0=0°,TX1=0°
Chirp1:TX0=0°,TX1=180°
Chirp0 and Chirp1 are all TX0 and TX1 EN=1.
Now i capture a adc data and postproc it. Results can be seen in fig2 and fig3.
first i cannot see the BMP config information in the programmed parameters at the right side of postproc window. Where is the BMP information? how can i confirm the config is right?
second how can i observe the difference between 0° and 180° in the plot?