I'm using the AWR1642BOOST which has 2T4R.
But I only use one TX.
After I read two white paper below:
Introduction to mmwave Sensing: FMCW Radars:
I tried the conversion of coordinates in the document.
And got the result.
I transformed the time bins of X-axis and four RX idx of Y-axis into range and degree respectively.
1. According to the www.ti.com/.../tidud36b.pdf
Antenna Field of View is ±60º With Angular Resolution of Approximately 15º
But in "Introduction to mmwave Sensing: FMCW Radars", Antenna Field of View is ±90º
And the maximum value of Y-axis in my simulation result is only 45 degree.
Is there anything wrong with the coordinates conversion formula?
2.Can you tell me how can you derive the FOV ±60º and Angular Resolution of Approximately 15º?
Thanks a lot!