Other Parts Discussed in Thread: AWR1443
After flashing the demo binary, I removed the SOP2 jumper and reboot the EVM. I use the online visualizer and try to run the demo, after selecting the SDK version and the platform, I click the "Send config to mmwave device", and I get the error as below. The guide says that if everything works fine, the console should end with "sensorstart" and "Done", but in my case the sensorstart returned with -1 and there is no error message. I am not sure which config is wrong, but I didn't change any of the config after selecting the platform and SDK version.
Also, I am using the sdk_01_02_00_05, and I am not sure this is version 1.2 or not, if it is not, then where can I get a sdk 1.2? The previous version of the latest sdk online is the 2.0 then is this sdk_01_02_00_05.
Thank you very much