Hello,
We have built an exact replica of the AWR1642BOOST with the only exception being a custom antenna.
The TM4C129 on the board is there to facilitate the USB connection to a PC.
With our custom board, the TM4C129 does not have the XDS110 firmware loaded to establish that USB connection.
I am assuming we need to JTAG into the TM4C129 and flash that firmware onto the MCU. However, the JTAG pins are not broken out at all.
- Is there anyway to flash the FW onto the MCU without reworking the board?
- Did TI flash the MCU after it was on the board? Or did we populate the board we pre-programmed MCUs?
Thank you,
Ryan B.