Any update on a fix to this issue on being unable to use both Tx antennas at the same time?
"The demo is not returning data because there is a bug in the software. The value numAntenna is used in the direction of arrival calculation. This value is the number of virtual antennas, which is Tx*Rx. However, when using both Tx at the same time, the 2 Tx are effectively 1 Tx for the virtual array. The software does not account for this, leading to a crash. The numAntenna value is set at line 1171 in dss_data_path.c. This value is used erroneously at line 350 in radarProcess.c."
Thanks,
Scott