Other Parts Discussed in Thread: AWR1642
Recently, I have tried to analyze some data from mmWave Demo Visualizer 3.0. But I have a problem about the sampling rate of the sensor.
After I start the sensor, the chirp/frame information in the plot tab shows that:
According to this, there are 256 samples/chirp, 16 chirps/frame, and 10 frames/second. Hence, I can obtain there are 256*16*10=40960 samples/second. Does it mean the sampling rate?
On the other hand, from the figure above, the sampling rate is presented as 5.209Msps. Does sps mean samples per second? If so, why this value is different from the value above?
Moreover, I am confused with the definition of 'sample'. It seems this 'sample' is different from 'sampling points' in sampling theorem. Since the frequency of radar sensor is between 77 and 81 GHz, the sampling rate should be larger than 162GHz according to Nyquist rate.
Would someone please help me to solve this confusion? Thank you very much.