Hi,there is strange phenomenons with AWR1243.the radar has two transmitting antennas,one is high gain antenna(26dB),another one is low gain antenna(18dB).The radar is 0.5m away from a car and there is nothing else around.The radar and the car are both static.
When the high gain antenna is opened and low gain is closed,a lot of false targets are detected,for example,35m&70km/h,50m&65km/h,102m&46km/h.
When the high gain antenna is closed and low gain is opened, very few false targets are detected.
It seems the false alarm is related to signal strength.
Do you have advice to solve this problem.Thank you