This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Single chip board Design is Available?

Part Number: IWR6843
Other Parts Discussed in Thread: MMWAVEICBOOST,

now what we have sensor  is ,we need to plugin the antenna module to the chip set. whether single chip IWR 6843 board  is Available or not?

  • Hi Manjunatha,

    Just to clarify, are you asking whether we have a single board EVM for IWR6843 instead of the Carrier Card (i.e. MMWAVEICBOOST) + Antenna Module (i.e. IWR6843ISK) offering?

    Thanks
    -Nitin
  • Manjunatha,

    We haven't heard back from you. Please note that we do not have a single board EVM for the IWR6843. The evaluation solution (i.e. the Industrial Starter Kit Bundle) consists of two boards, the MMWAVEICBOOST i.e. the Industrial carrier platform and the IWR6843ISK which is the Standard long range antenna module using the IWR6843 mmwave device.  The MMWAVEICBOOST carrier platform allows flexibility in evaluation as you can plug-in different antenna modules which could be designed for different application requirements.

    However, there are various third party mmWave modules designed and supported directly by our Ecosystem partners. You can find more information about the modules including the corresponding ecosystem partner link at the following page:

    mmWave Modules

    Thanks

    -Nitin