Hi,
HW: AWR1642
SW: mmWave SDK 2.1
We're testing Tx ball break monitoring.
No matter on TI AWR1642 EVM or customer EVM, we got around 1.6 dB difference between these 2 Tx.
The value we get is from TX_REFL_COEFF_VALUE inside AWR_MONITOR_TXn_BALLBREAK_REPORT_AE_SB (Refer to DFP)
The 2 value from different 2 Tx are -118=-11.8dB ,-102=-10.2 dB
Is this a normal result? (We expect the difference would be very small)
If this is not a normal result, what could be the reasons behind to lead so much difference?