I'm demonstrating gesture using IWR1443BOOST and mmwave_industrial_toolbox_2_5_2.
I have some questions about matlab script "plot_gesture_twirl.m" in "mmwave_industrial_toolbox_2_5_2\labs\lab0009-gesture-recog-twirl\gui".
There are ten matrix in "plot_gesture_twirl.m" as below;
numdetections
numdetectionspos
numdetectionsneg
dopplerave
doppleravepos
doppleraveneg
rangeave
magsum
angleval
rangeidx
1)Please let me know the meaning of each matrix.
I assume the meaning of the following matrix. Are my assumptions correct?
dopplerave: Average of speed of moving hand measured by radar.
rangeave: Average of Range[Distance] to hand measured by radar.
angleval: Value of angle of hand position measured by radar.
2)Regarding "numdetections", "dopplerave", "magsum" and "rangeidx",
these are not used to determine gesture in the script, right?
Please advise.