I tried to increase the sampling rate by reducing the the Periodicity (ms) parameters under the Frame configuration section.
When I ran the scrip with these configurations:
ar1.FrameConfig(0, 1, 0, 1, 0.25, 0, 2)
I got the following error:
Frame duration programmed is 0.25 ms Frame duration needed is 0.2532 ms ERROR: Frame duration programmed is less than what is actually needed!
What other settings do I need to tweak so that the frame duration needed can be lower?