Other Parts Discussed in Thread: IWR6843, , MMWAVEICBOOST
Tool/software: Code Composer Studio
Hi,
Can you provide which GPIO are available at the IWR6843 ISK board ?
Also, some code for IO control of such ports ?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi,
Can you provide which GPIO are available at the IWR6843 ISK board ?
Also, some code for IO control of such ports ?
Thank you
Hi charles.
Thank you for the answer.
I've asked for assistance in locating free io when the iwr6843 is mounted on the boost board.
At the initial answer ,you mentioned that gpio0/1/2 are free, but according to schematics,they are connected to peripherals on the boost board.
Please direct .
Gil
Hi Again,
my intention is to control LED through the available IO's.
connect wires to the IO, and to external small circuit.\that contains the LEDs
Gil