I need help with figuring out for the TMP75/175AIDR what the RH value maximum is for humidity. I am operating at 70%-90% RH. Is it okay to use potting material to insulate the pins and the chip or will it degrade the accuracy?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need help with figuring out for the TMP75/175AIDR what the RH value maximum is for humidity. I am operating at 70%-90% RH. Is it okay to use potting material to insulate the pins and the chip or will it degrade the accuracy?
Hi Steven,
I don't believe we have any specific guidelines for the temperature sensing products regarding RH exposure. Are you concerned about corrosion?
Potting material will change the thermal performance, but it's hard to say if the change would be a boon or a hindrance in your application. If you're trying to measure the temperature of a specific location or object, potting material may improve thermal conduction between the sensor and the object of interest. If you're trying to measure ambient air temperature, then any additional thermal path or thermal insulation will likely worsen the thermal performance.
Thanks,
Ren
This sensor will be sitting on top of a heat sink. The worry I have is the effective vomtage mesured due to the humidity. Typical applications I have used this in humidity was not an issue. I just need to know if humidity will cause acvuracy issues or if potting will?
Will this device be okay to have potting material on it or will that cause degridation of the accuracy or another issue?
Hi Steven,
I don't expect the device itself to be altered by potting material. Adding thermal mass to the system will have some effect on system thermal performance regardless of the sensor used.
Thanks,
Ren