Other Parts Discussed in Thread: MMWCAS-RF-EVM
Hi,
In according with the application report AWR1243 Cascade I have some question:
It is possible to have gerber information about the 20GHz LO sync (See the document: Cascaded Radar And Body&Chassis Automotive Applications)?
I have the position of the TX and RX antenna on the PCB similar with the MMWCAS-RF-EVM board (See the document: Cascaded Radar And Body&Chassis Automotive Applications), so the 20 GHz line must be routed on the internal layer,
the only way not to interfere with the antenna lines, positioned on the top, is to think of a 20GHz stripline on internal layers using a second dielectric. Is it a correct solution?
I have a second question, in attacched file is reporded my scheme of a two chip cascade, it is correct?
ThanksAWR1243_cascade.docx