This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

IWR1443: Program the IWR1443 using TMDSEMU110-U

Expert 2865 points

Replies: 19

Views: 571

Part Number: IWR1443

Hello,

I have a IWR1443 based custom PCB which I am trying to program using TMDSEMU110-U. I have connected UART port RX and TX to corresponding Auxillary port TX and RX and have connected a common GND. I have ensured SOP setting to the flasing setting. I am unable to program using UNIFLASH. It says it is unable "Not able to connect to serial port". Are these connections and my procedure correct to load the program?

Regards,

Prudhvi Sagar

  • Hi Prudhvi,

    I'll need to discuss this with our hardware team. We should have an answer for you sometime next week.

    Cheers,

    Akash

  • Hi Prudhvi,

    sounds like you are following the right steps.

    1. Can you confirm if the COM port is showing up as expected?
    2. After setting the SOP mode are you resetting the board?
    3. Do you have the right COM port in UNIFLASH
    4. Lastly, Can you confirm you don't have the COM port opened on any other application?

    Regards,

    Charles O

     

  • In reply to Charles Oladimeji:

    Hello,

    I can confirm all the steps you have mentioned. Today I tested on my IWR1443BOOST by populating R166 and R169 and connecting  AR_RS232TX and AR_RS232RX from J5 to my debugger. I have additionally connected GND and also powered my device. I am still unable to succeed.

    [7/22/2019, 4:50:33 PM] [INFO] Cortex_R4_0: Initialization complete.
    [7/22/2019, 4:50:33 PM] [INFO] Cortex_R4_0: Flashing process starting...
    [7/22/2019, 4:50:33 PM] [INFO] Cortex_R4_0: Connecting to COM Port COM24...
    [7/22/2019, 4:50:33 PM] [INFO] Cortex_R4_0: Reset connection to device
    [7/22/2019, 4:50:33 PM] [INFO] Cortex_R4_0: Set break signal
    [7/22/2019, 4:50:54 PM] [ERROR] Cortex_R4_0: Initial response from the device was not received. Please power cycle device before re-flashing.
    [7/22/2019, 4:50:54 PM] [ERROR] Cortex_R4_0: Not able to connect to serial port. Recheck COM port selected and/or permissions.
    [7/22/2019, 4:50:54 PM] [INFO] Cortex_R4_0: Flashing instance clean-up initiated...
    [7/22/2019, 4:50:54 PM] [INFO] Cortex_R4_0: Instance deinitialized!
    This is the output I am getting. Is there anyway to check my debugger?
    Regards,
    Prudhvi Sagar
  • In reply to Prudhvi Sagar:

    Hi,

    When you connected the RX pins to your debugger, did you removed the resistors routing the UART to the onboard XDS110?

    Regards,

    Charles O

     

  • In reply to Charles Oladimeji:

    Hello,

    No I haven't removed them. I can try with them removed tomorrow.

    Regards,

    Prudhvi Sagar

  • In reply to Charles Oladimeji:

    Hello,

    I have tried after depopulating the UART resistors aswell. Still I am unable to succeed. Same behavior is being repeated. I am confused as in what the issue is. Do you think the connecting cables are causing the issue? I am in a process of making a custom PCB and am confused to how would I program it.

    Regards,

    Prudhvi Sagar

  • In reply to Prudhvi Sagar:

    Hi,

    The issue shouldn't be caused by the cable.

    Can you try programming the board using the onboard XDS110 and then sending the config and data using the emulation board to confirm if its an issue of compatibility with Uniflash?

    Regards,

    Charles O

     

  • Genius 12475 points

    In reply to Prudhvi Sagar:

    Hello Prudhvi,

    You can also just use a USB to FTDI cable instead of the XDS110 debug probe.

    https://www.alliedelec.com/product/ftdi/ttl-232r-rpi/70403954/?gclid=EAIaIQobChMI-pXD05fv4wIVYP_jBx0rBQ7vEAQYAyABEgIE2fD_BwE&gclsrc=aw.ds

    We have tested this solution and had no issues. 

    Regards,

    Adrian

  • In reply to aozer:

    Hi,

    I assume you were able to resolve this and will be closing the thread. Please reply if you still need assistance or make a new post referencing this one.

    Regards,

    Charles O

     

  • In reply to Charles Oladimeji:

    Hello,

    I am still trying and unable to succeed. I am unsure how to program the board and confused how to give pins tp flash for a custom PCB.

    Regards,

    Prudhvi Sagar

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.