This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

FDC2214: Using FDC2214 and LDC1101 together for proximity sensor.

Prodigy 110 points

Replies: 2

Views: 89

Part Number: FDC2214

I have made a custom board with FDC2214 and LDC1101 inside.

I am trying to use LDC1101 and FDC2214 simultaneously by attaching different sensors.

When I activate only FDC2214, the proximity sensing works.

However, when I activate both LDC101 and fDC2214, the proximity sensing for both does not work.

No line is shared between LDC1101 and FDC2214, but this happens.

Why is this happening?

  • Hello,

    If the sensors are too close, their resonant frequencies may be interfering with each other. Please also double-check that your power supply can support both the LDC1101 and the FDC2214 running simultaneously. 

    Best Regards,

    Kristin Jones

    Current and Position Sensing

    Applications Engineer

    For more information, check out the Inductive Sensing FAQ

  • In reply to Kristin Jones93:

    Hello,

    I haven't heard from you in a while, so I'm assuming you were able to resolve your issue. If this is not the case please feel free to reply to this thread or post a new question.

    Best Regards,

    Kristin Jones

    Current and Position Sensing

    Applications Engineer

    For more information, check out the Inductive Sensing FAQ

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.