Other Parts Discussed in Thread: HDC2080
Team,
Where is R12 on the HDC2080EVM?
We are switching addresses from 0x40 to 0x41 via a resistor as outlined in section 2.2 of this document (attached).
The I2C address of the HDC2080 is set at EVM level at 1000000xb on the EVM. The I2C address has
been set mounting the 0 Ω resistor R12 (refer to Figure 2).
Can’t see R12 anywhere in the pictures or on the actual board.
Thank you.