As per the datasheet specification, LM35CZ senses from -40 to 110 deg Celsius. If the temperature is negative, whether the output of the sensor is negative as per transfer function?
Eg: If Temp = -20deg C
Then VOUT = 10mV / deg C * (-20) = 200mV
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As per the datasheet specification, LM35CZ senses from -40 to 110 deg Celsius. If the temperature is negative, whether the output of the sensor is negative as per transfer function?
Eg: If Temp = -20deg C
Then VOUT = 10mV / deg C * (-20) = 200mV
Hi Jalen
You mean circuit implementation will change for -ve temperature monitoring but the transfer will still remain the same?
Regards
Srikanth Kacchu
Srikanth,
Yes that is correct. You essentially need to be able to pull the voltage below ground (the negative rail) in order to output voltage corresponding to negative temperatures.
Jalen