Hi,
I am trying to open mmWaveStudio through the following windows command line (note that environment variables have include the mmWaveStudio installation path):
START /B mmWaveStudio.exe
However, I always get the following error message:
GM: Constructor
GM: Fri Sep 13 18:03:48 2019
RSTD.Transmit("/Settings")
[18:03:49]
[18:03:49] ### Running Startup script: "C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Scripts\Startup.lua" ###
[18:03:49] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[18:03:49] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[18:03:49] Scripter ignored: Attempt to UnBuild() again or before Build.
[18:03:49] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[18:03:49] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[18:03:49] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[18:03:49] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[18:03:49] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[18:03:49] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[18:03:49] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_01_00_00_00\\mmWaveStudio\\RunTime\\SAL.dll")
[18:03:49] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[18:03:49] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[18:03:49] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[18:03:49] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[18:03:49] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[18:03:49] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[18:03:49] RSTD.Transmit("/")
[18:03:49] RSTD.SaveSettings(): Settings saved to "C:\Users\Weite\AppData\Roaming\RSTD\config.xml"
[18:03:49] RSTD.Build()
[18:03:49] RSTD.SaveSettings(): Settings saved to "C:\Users\Weite\AppData\Roaming\RSTD\config.xml"
[18:03:49] RSTD.Transmit("/")
[18:03:49] RSTD.AL_Build()
[18:03:49] RSTD.AL_LoadXml()
[18:03:49] RSTD.Transmit("/")
[18:03:49] RSTD.AL_Init()
[18:03:49] RSTD.Clients_Build()
[18:03:49] GM: Init
[18:03:49] GM: Loaded 'C:\ti\mmwave_studio_01_00_00_00\mmWaveStudio\Clients\\LabClient.dll'
[18:03:49] GM: 1 Guest (s) init
[18:03:49] GM: 1 Module(s) init
[18:03:49] GM: 2 Tab (s) init
[18:03:49] RSTD.Client_LoadXml()
[18:03:49] [RadarAPI]: Starting Matlab Engine..
[18:03:52] [RadarAPI]: Error:
[18:03:52]
[18:03:52] ... MWMCR::EvaluateFunction error ...
[18:03:52] Invalid file identifier. Use fopen to generate a valid file identifier.
[18:03:52] Error in => Initialize_PostProcEngine.m at line 102.
[18:03:52]
[18:03:52] ... Matlab M-code Stack Trace ...
[18:03:52] at
[18:03:52] file C:\Users\Weite\AppData\Local\Temp\Weite\mcrCache8.5.1\Matlab0\MatlabPostPr\Initialize_PostProcEngine.m, name Initialize_PostProcEngine, line 102.
[18:03:52]
[18:03:52]
[18:03:52] Trace:
[18:03:52] at MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(String functionName, Int32 numArgsOut, Int32 numArgsIn, MWArray[] argsIn)
[18:03:52] at MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(Int32 numArgsOut, String functionName, MWArray[] argsIn)
[18:03:52] at MatlabPostProcGui.MatlabPostProcGUIClass.Initialize_PostProcEngine(MWArray BaseFolder)
[18:03:52] at AR1xController.frmAR1Main.InitMatlabPostProcEngine(String PostProcesspath)
[18:03:52] [RadarAPI]: Error: Error occured in Matlab Initialization
[18:03:52] [RadarAPI]: Matlab Engine couldn't be Started..
[18:03:56] [RadarAPI]: ar1.LoadSettings('C:\Users\Weite\AppData\Roaming\RSTD\ar1gui.ini')
[18:03:56] [RadarAPI]: Error:
[18:03:56]
[18:03:56] ... MWMCR::EvaluateFunction error ...
[18:03:56] Attempt to reference field of non-structure array.
[18:03:56] Error in => postProcVersion.m at line 3.
[18:03:56]
[18:03:56] ... Matlab M-code Stack Trace ...
[18:03:56] at
[18:03:56] file C:\Users\Weite\AppData\Local\Temp\Weite\mcrCache8.5.1\Matlab0\MatlabPostPr\postProcVersion.m, name postProcVersion, line 3.
[18:03:56]
[18:03:56]
[18:03:56] Trace:
[18:03:56] at MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(String functionName, Int32 numArgsOut, Int32 numArgsIn, MWArray[] argsIn)
[18:03:56] at MathWorks.MATLAB.NET.Utility.MWMCR.EvaluateFunction(String functionName, MWArray[] argsIn)
[18:03:56] at MatlabPostProcGui.MatlabPostProcGUIClass.postProcVersion()
[18:03:56] at AR1xController.ScriptOps.getMatlabPostProcVersion()
[18:03:56] TESTING = false
[18:03:56] RstdNet: Port 2777: Listening..
[18:03:56] Open a listening server on port 2777
[18:03:58]
[18:03:58] ***Script completed successfully.***
Could you give me some advices?
Thank you,
Weite