hi,
1)、Use the SDK to calibrate opt3101. When initializing the settings, put "monoshot_mode=3". Read when performing crosstalk calibration,the crosstalk value is all "0". Is this a normal phenomenon? If it is normal, it means that "monoshot_mode=0" is required before performing the crosstalk calibration operation, right?
2)、Some of the descriptions in Section 4.2.3 (Scale Value for Crosstalk Measurement) are in the “OPT3101 Distance Sensor System Calibration” manual. such as:
1. "A system with crosstalk greater than 32768 × 1.64676 / 2⁶ = 843" How did "32768" and "1.64676" come from?
2. "Typically expected crosstalk is < 200 codes with highest LED current" means mask photodiode and measure the amplitude: AMP_OUT register<200?
3.mask photodiode and measure the Amplitude: The AMP_OUT register value is approximately 15000. Will the crosstalk calibration be invalid? How can I confirm that the crosstalk calibration is successful?
Best,
dongming.cui