Tool/software: Code Composer Studio
Hi Ti,
I recently is working on migrating my PPL project(base to lab0020_pplcount_Overhead) to ES2.0 from ES1.0. I can output adc raw data through lvds on es1.0,and all the initiate code about lvds(eg. CBUFF, EDMA,ADCBUF)is on dss project.But when I migrated the same code to ES2.0, the adc raw data can't output through lvds. I checked the CBUFF registers, found that all of the cbuff registers value is zero.Then I checked the return value of invoking CBUFF_init, it is not null, it is success .Why I can success invoke CBUFF_init function, but the cbuff registers wasn't setted?