This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Problem with DCA1000EVM and mmWave Studio 2.0.0.2

Part Number: DCA1000EVM
Other Parts Discussed in Thread: IWR6843ISK, , MMWAVEICBOOST

Dear all,

I recently got IWR6843ISK + MMWAVEICBOOST + DCA1000EVM. The boards are powered from the MMWAVEICBOOST board (I use a lab power supply 5V, 5A).

I followed the "DCA1000EVM Quick Start Guide" and "DCA1000EVM Data Capture Card" user's guide but I have issue with the DCA1000EVM. I guess it is in controlling the Ethernet. 

Those are the settings I'm using.

For MMWAVEICBOOST

For DCA1000EVM

Are those settings correct?

I have already programmed the FPGA SPI Flash using Lattice Diamond and DCA1000_FPGA_RECORD_V2.7_18JUN2018.bit 

I got this issue when I try to click on "Connect, Reset and Configure":

Is it normal that the FPGA Version is 0.0.0.0? I programmed many times the FPGA SPI Flash but still the same issue.

I tried other configurations of the DCA1000EVM but the problem is still there. For example, I used HD_CONFIG (SW2.5), Loading the Ethernet configuration data from EEPROM (SW2.6 to USER_SW1), ...

This is when I try DataCaptureDemo_xWR:

If I click on (1) to (6), it seems working but still failing when I click "SetUP DCA1000".

Here are some screenshots of Wireshark:

Thanks a lot in advance.

Best Regards,

Marco