This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01012: Config/Data Capture without mmWave Studio

Part Number: TIDEP-01012
Other Parts Discussed in Thread: TDA2SX, DCA1000EVM, AWR1243BOOST, AWR1243, TIDEP-01017, MMWCAS-DSP-EVM

Hello,

 

We’re looking to get the cascade radar eval kit (RF-EVM / DSP-EVM) integrated into ROS (running in Linux) so that we can do some sensor fusion of it with a camera and lidar feed. The main issues I can see with this are:

  1. How to communicate with the TDA2SX processor on the DSP-EVM board to enable data capture without mmWave Studio? Is there any example source code available for this? I know that for the DCA1000EVM data capture board that is used to capture ADC data from the single-radar chip eval boards there is an application available in Windows/Linux to control this without mmWave Studio – http://e2e.ti.com/support/sensors/f/1023/t/856054?-FAQ-Raw-ADC-data-Capture-from-mmWave-Sensor/ Q11. Also there's sample code in the rf_api.h header file supplied with mmWave Studio, however I'm not aware of anything similar for the cascade radar though.

  2. How to communicate with the TDA2SX SoC on the DSP-EVM board to enable setup of the 4 x AWR1243P chips on the RF-EVM board without mmWave Studio? Is there any example source code available for this? For the single-chip eval boards (e.g. AWR1243BOOST) there is the mmWaveLink example source code (using mmWave Studio dll file) available in the Device Firmware Package that can be used to set up the AWR1243 chip over the USB-SPI link enabled by FTDI chip on DCA1000EVM board. Again I'm not aware of anything similar for the cascade radar though.

  3. Transferring of files from the SSD on the DSP-EVM board onto the PC/laptop is very slow, can this be speeded up in some way to make the capture closer to real-time or at least with lower latency?

I'm thinking we'll have to just write our own firmware for the TDA2SX processor to do (1-2) above, which is what we'd intend to do long-term anyhow but just would be good if there was a Linux-compatible solution for demos in shorter-term. 

Best regards,

Peter.