Hi,
Are there any S22's (Transmit) looking into the AWR1843? I have found on page 30 of the datasheet that the S11 is <-10dB.
Also, on the AWR1843 is the digital beam forming on RX true time delay?
Thanks,
Kathleen
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Are there any S22's (Transmit) looking into the AWR1843? I have found on page 30 of the datasheet that the S11 is <-10dB.
Also, on the AWR1843 is the digital beam forming on RX true time delay?
Thanks,
Kathleen
Hello Kathleen,
The return loss looking into the TX port is also <-10dB. You can refer to the following post to get more details of the Rx and Tx S11 and S22 values : https://e2e.ti.com/support/sensors/f/1023/p/637734/2383257
That post is related to 1243 but the impedances for 1243 and 1843 are the same.
Regards,
Vivek