Have a couple of questions regarding the SRR demo object output:
1) What is the grid size (number of range bins and azimuth bins) of the SRR objects those are available in the TLV. In the TLV only the detected objects, clusters and tracked output locations are provided.
I understand that the grid size (in range) is determined by the range fft size, that can be scaled properly using the formula (fs/N)*k where fs is beat (ADC) sampling frequency, N is the range FFT size and k =1:N is the range FFT output sample index. Similarly, the grid size (along azimuth angle direction) is determined by the FFT size that can be scaled using the formula asin(2*kmax/M) where asin is inverse sin, M is azimuth fft size, kmax=1:M is the azimuth fft output bin index.
where are the range and azimuth FFT sizes been declared in dss_data_path.c ?
2) Will the grid sizes for SRR and USRR subframes be different. How is a TLV frame for SRR demo populated. Is it alternating between SRR and USRR or the USRR subframe data (till 20 m) is superposed or combined with that of SRR subframe (assuming it to be till 80 m).