Other Parts Discussed in Thread: MMWAVE-SDK
HW: AWR1843BOOST Rev. C and Rev. B
SW: SBL in mmWave SDK 3.2
We use the binary (SBL in mmWave SDK 3.2) to do firmware downloading test via CAN-FD and found a strange symptom:
- The CAN-FD 5Mbps Tx fail sometimes (The reproduce rate is around 1/3 and it means firmware downloading fail one time when you try three times) on AWR1843BOOST Rev. C EVM
- The CAN-FD 5Mbps Tx works fine on AWR1843BOOST Rev. B EVM
We perform more test and the found: If we lower the speed from 5Mbps to 2Mbps on Rev. C EVM, it always work.
Base on the test result we suspect AWR1843BOOST Rev. C EVM "may" have layout issue related CAN-FD.
Do you have any comment?