Other Parts Discussed in Thread: IWR1443, DCA1000EVM, IWR1443BOOST, IWR1243, UNIFLASH
Hi,
I've been using an IWR1443 device with DCA1000EVM for a while, and recently I started running into the issue I mentioned in the title. I follow the procedure to upload BSS/MSS firmware, and when I click SPI Connect in mmWave Studio, I receive the error: RESP TIMEOUT: MSS Power Up async event was not received.
I've tried resetting SFLASH a couple of times, and it does not solve my problem. I'm connecting to device in SOP2 mode (SOP0 and SOP1 has jumpers, SOP2 port hasn't). I also know that my firewall is turned off, and I run mmWave Studio as an administrator.
Lastly, I've also tried flashing a different firmware, vital signs monitor for the device, and it seems that the demo is also working perfectly fine. I did not run into any errors while flashing the demo firmware.
I've also tried other solutions in the forum, but they did not seem to help. I also have a power adapters that are rated at 5V, 3A; thus, they should not be an issue. (Everything was working some time ago anyways).
I've attached the log files
GM: Constructor GM: Thu Feb 20 14:28:16 2020 RSTD.Transmit("/Settings") [14:28:16] [14:28:16] ### Running Startup script: "C:\ti\mmwave_studio_02_01_00_00\mmWaveStudio\Scripts\Startup.lua" ### [14:28:16] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1") [14:28:16] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss") [14:28:16] Scripter ignored: Attempt to UnBuild() again or before Build. [14:28:16] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Clients\\\\LabClient.dll") [14:28:16] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE") [14:28:16] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE") [14:28:16] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE") [14:28:16] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE") [14:28:16] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE") [14:28:16] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\RunTime\\SAL.dll") [14:28:16] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "") [14:28:16] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE") [14:28:16] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1") [14:28:16] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE") [14:28:16] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE") [14:28:16] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false") [14:28:16] RSTD.Transmit("/") [14:28:16] RSTD.SaveSettings(): Settings saved to "***********\AppData\Roaming\RSTD\config.xml" [14:28:16] RSTD.Build() [14:28:16] RSTD.SaveSettings(): Settings saved to "***********\AppData\Roaming\RSTD\config.xml" [14:28:16] RSTD.Transmit("/") [14:28:16] RSTD.AL_Build() [14:28:16] RSTD.AL_LoadXml() [14:28:16] RSTD.Transmit("/") [14:28:16] RSTD.AL_Init() [14:28:16] RSTD.Clients_Build() [14:28:16] GM: Init [14:28:16] GM: Loaded 'C:\ti\mmwave_studio_02_01_00_00\mmWaveStudio\Clients\\LabClient.dll' [14:28:16] GM: 1 Guest (s) init [14:28:16] GM: 1 Module(s) init [14:28:16] GM: 2 Tab (s) init [14:28:16] RSTD.Client_LoadXml() [14:28:17] [RadarAPI]: ar1.selectRadarMode(0) [14:28:17] [RadarAPI]: Status: Passed [14:28:17] Matlab Runtime Engine is installed [14:28:17] [RadarAPI]: Starting Matlab Engine.. [14:28:18] [RadarAPI]: Matlab Engine Started! [14:28:19] [RadarAPI]: ar1.selectCascadeMode(0) [14:28:19] [RadarAPI]: Status: Passed [14:28:19] [RadarAPI]: ar1.LoadSettings('***********\AppData\Roaming\RSTD\ar1gui.ini') [14:28:20] TESTING = false [14:28:20] RstdNet: Port 2777: Listening.. [14:28:20] [14:28:20] ***Script completed successfully.*** [14:28:22] [RadarAPI]: Opening Gpio Control Port() [14:28:22] [RadarAPI]: Status: Passed [14:28:23] [RadarAPI]: Opening Board Control Port() [14:28:23] [RadarAPI]: Status: Passed [14:28:24] [RadarAPI]: ar1.FullReset() [14:28:24] [RadarAPI]: Status: Passed [14:28:25] [RadarAPI]: Closing Board Control Port() [14:28:25] [RadarAPI]: Status: Passed [14:28:25] [RadarAPI]: Closing Gpio Control Port() [14:28:25] [RadarAPI]: Status: Passed [14:28:25] [RadarAPI]: ar1.SOPControl(2) [14:28:25] [RadarAPI]: Status: Passed [14:28:26] [RadarAPI]: ar1.Connect(4,921600,1000) [14:28:27] [RadarAPI]: ar1.Calling_IsConnected() [14:28:28] [RadarAPI]: ar1.SelectChipVersion("AR1243") [14:28:28] [RadarAPI]: Status: Passed [14:28:28] [RadarAPI]: ar1.SelectChipVersion("AR1243") [14:28:28] [RadarAPI]: Status: Passed [14:28:28] [RadarAPI]: ar1.deviceVariantSelection("XWR1443") [14:28:28] [RadarAPI]: Status: Passed [14:28:28] [RadarAPI]: ar1.frequencyBandSelection("77G") [14:28:28] [RadarAPI]: ar1.SelectChipVersion("XWR1443") [14:28:28] [RadarAPI]: Status: Passed [14:28:28] Device Status : XWR1443/QM/SOP:2/ES:3 [14:28:28] [RadarAPI]: ar1.SaveSettings('*********\AppData\Roaming\RSTD\ar1gui.ini') [14:28:30] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss.bin") [14:28:30] [RadarAPI]: Downloading BSS Patch RPRC Binary.. [14:28:32] [RadarAPI]: ar1.GetBSSFwVersion() [14:28:32] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17)) [14:28:33] [RadarAPI]: ar1.GetBSSPatchFwVersion() [14:28:33] [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19)) [14:28:33] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\masterss\\xwr12xx_xwr14xx_masterss.bin") [14:28:34] [RadarAPI]: Downloading MSS RPRC Binary.. [14:28:37] [RadarAPI]: ar1.GetMSSFwVersion() [14:28:37] [RadarAPI]: MSSFwVersion:(01.02.05.01 (12/07/19)) [14:28:43] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0) [14:28:43] Status: Failed, Error Type: RESP TIMEOUT [14:28:47] MSS Power Up async event was not received!
Thanks
Ps. I posted this by selecting 'ask a related question' on a forum post that had a similar problem with IWR1243; hence my part number shows up as 1243. I have IWR1443BOOST, as I mentioned in the post.